Panasonic PAN9320ETU Wi-Fi/802.11 Development Tool

Panasonic PAN9320ETU Wi-Fi/802.11 Development Tool contains an integrated web-stack that provides a lot of features. Connect the USB0 Port to the USB-Port at the development PC for powering up the PAN9320ETU. The USB1 is connected to the Uart1 of the module and features its Netcat TCP-Data-Tunnel capability. A DualRS232 FTDI chip is used on the board to provide a connection to the PAN9320 UART via virtual USB Com-Port.
Publicerad: 2016-01-11 | Uppdaterad: 2022-03-11