Mouser Interviews Uzi Hanuni, Developer of High-Tech Communication Solutions Invaluable in Saving Thai Soccer Team

För omedelbar lansering

Anslut till oss


Mouser talks to Uzi Hanuni of Maxtech Networks about the company's communications technology used in the Thai cave rescue of July 2018.

July 31, 2018 - The harrowing ordeal of a Thai soccer team trapped in a water-filled cave gripped the world's attention for more than two weeks in June and July 2018. It was a complicated and daring rescue, but little has been said about the amazing technology that helped make their rescue possible.

Mouser Electronics recently had the rare opportunity to speak with Uzi Hanuni, founder and CEO of Maxtech Networks, to learn more about the company's innovative MaxMesh technology that was crucial in the rescue.

Rescuers faced many challenges after locating the trapped boys and their coach in the Tham Luang Nang Non cave in Thailand. Normal radio signals were blocked by cave walls. Water from the monsoon season posed additional challenges. Learning of the situation, Hanuni dispatched an engineer and several of his MaxMesh radios to the scene. Hanuni's revolutionary system essentially established a relay network throughout the two miles of twists, turns and partially submerged areas of the tunnel, enabling rescuers to connect, share, collaborate and ultimately bring the team to safety.

"Our technology is based on creating a mesh network of software-defined radios [SDRs]. SDRs are radio communication systems using software on a personal computer or embedded system," Hanuni explained. "Every time you switch on a radio, it automatically joins the network. Each radio is also a relay, and the intelligent frequency modulation algorithms are built into the radios. They can transmit video, voice and data simultaneously."

Hanuni's interest in devising a better form of communication technology arose after the attacks of Sept. 11, 2001, as he saw many first responders cut off after the World Trade Center towers collapsed and their radio antennas were damaged.

"I thought the technology we needed to develop had to work automatically so that you switch on the radio and suddenly it's connected — peer-to-peer groups, multicast, unicast, broadcast, whatever you want. And you have it there with no need to preconfigure the radios," Hanuni continued. "It took us a few years to develop the sophisticated algorithm and the technology that works indoors, outdoors, underground, above ground, in all places automatically with no human interference or involvement.

"Our technology can be encapsulated in various forms. The Mini PCI Express card [we use] is our own technology, only it has a field-programmable gate array (FPGA). This is the key fundamental component. We are using the Analog Devices AD9364 high-performance, highly integrated radio frequency Agile transceiver for communications. In addition, we are also using the Artix-7, which is a device that offers great performance for high-end gateways with local processing and analytics to improve latency and responsiveness. With the Artix-7 is an Intel® Cyclone® III FPGA."

To watch the full interview with Uzi Hanuni, go to https://youtu.be/xCvy_IeKXNU. For a deeper exploration of the Maxtech Networks technology, visit www.mouser.com/applications/cave-rescue-technology.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764