Terasic’s DE10-Nano Kit, Built on the Intel Cyclone V FPGA, Now at Mouser Electronics

Nya produktlanseringar

Anslut till oss


Terasic’s DE10-Nano Kit, Built on the Intel Cyclone V FPGA, Now at Mouser Electronics

July 27, 2017 - Mouser Electronics, Inc., the New Product Introduction (NPI) leader that empowers innovation, is now stocking the DE10-Nano development kit from Terasic Technologies, a platinum member of the Intel® FPGA Design Solutions Network. The DE10-Nano kit is a robust hardware design platform built around an Intel System-on-Chip (SoC) FPGA, which combines a processor, peripherals, and an FPGA fabric into a single, user-customizable device.

The Terasic DE10-Nano kit, available from Mouser Electronics, is based on the 28 nm Intel Cyclone® V SoC FPGA, which integrates dual-core ARM® Cortex®-A9 embedded cores with industry-leading programmable logic for maximum design flexibility. Developers can leverage the power of reconfigurability along with a high-performance, low-power processor system. The Cyclone V SoC combines an ARM-based hard processor system (HPS) consisting of processor, peripherals, and memory interfaces tied seamlessly with the FPGA fabric using a high-bandwidth interconnect backbone.

The DE10-Nano kit includes two 40-pin general-purpose input/output (GPIO) headers, 1 GByte of high-speed DDR3 memory, a 12-bit analog-to-digital converter (ADC), Gigabit Ethernet networking, and an HDMI transmitter. The kit contains all the components required to use the board with a computer running Microsoft Windows XP or later.

To learn more about the DE10-Nano development kit, visit http://www.mouser.com/new/terasic-technologies/terasic-de10-nano-kit/.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Terasic Technologies

2026 - Terasic Technologies offers expertise in FPGA/ASIC design, high speed board design and layout, low cost board design, device drivers, and all other supporting software and documentation. They are dedicated to providing a wide range of various FPGA based boards for academia and industries. Terasic's cutting-edge design and manufacturing capabilities provide state of the art products and exceptional services to their customers. Terasic products have enjoyed phenomenal success all over the world and continues to set the standard in development hardware.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764