Mouser Electronics Now Offering Full UWB (formerly Decawave) Portfolio from Qorvo

Nya produktlanseringar

Anslut till oss


Mouser Electronics Now Offering Full UWB (formerly Decawave) Portfolio from Qorvo

September 29, 2020 - Mouser Electronics, Inc., an authorized global distributor of Qorvo products, is pleased to announce that Qorvo's complete line of ultra-wideband (UWB) technology products — formerly Decawave — is now available to order on the Mouser website. Qorvo's UWB product portfolio includes pioneering Impulse Radio UWB technology, which allows for centimeter accuracy distance/location measurement and secure low-power, low-latency data communication in automotive, mobile, industrial, and consumer Internet of Things (IoT) applications.

Qorvo, a leading provider of innovative RF solutions that connect the world, recently acquired Decawave, a pioneer in UWB technology and provider of UWB solutions for mobile, automotive and IoT applications. Decawave UWB products have successfully been deployed in more than 40 verticals, ranging from industrial automation to logistics, hospitals, cars, home robots, connected home, and sports. Decawave joined Qorvo as the Ultra-Wideband Business Unit (UWBU) within Qorvo Mobile Products.

Qorvo's line of UWB technology products, now available at Mouser, includes the DW1000 radio IC and two modules built around the DW1000 IC. The DW1000 UWB transceiver IC is the world's first single-chip wireless transceiver based on UWB techniques. The IC enables engineers to develop cost-effective real-time locating system (RTLS) solutions with precise indoor and outdoor positioning to within 10 cm. Compliant to IEEE802.15.4-2011, the IC supports data transfer at rates up to 6.8 Mbps.

The DWM1000 module integrates the DW1000 IC, an antenna, and power management and clocking components to simplify design integration with a wide variety of microcontrollers. The module supports time-of-flight (ToF) and time-difference-of-arrival (TDoA) location schemes in RTLS and wireless networking applications such as agriculture, building control, factory automation, and healthcare.

Qorvo's DWM1001 module combines the DW1000 IC, a Nordic Semiconductor nRF52832 system-on-chip (SoC), a 3-axis accelerometer, and integrated antennas to create a solution that minimizes RF and hardware design requirements. For development, Mouser stocks the DWM1001-DEV, which includes the DWM1001 module, battery connector and charging circuit, LEDs, buttons, Raspberry Pi-compatible connectivity, and USB connector. In addition, the board comes with J-Link OB adding debugging and Virtual COM Port capabilities.

For more information on Qorvo UWB technology products, visit https://www.mouser.com/new/qorvo/qorvo-uwb-technology/.

To learn more about Qorvo, go to https://www.mouser.com/manufacturer/qorvo/.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Qorvo

2026 - Qorvo supplies innovative semiconductor solutions and is a leading provider of connectivity and power solutions. As a global leader in RF and power, Qorvo combines product and technology leadership, systems-level expertise, and global manufacturing scale to quickly solve customers' most complex technical challenges. Qorvo serves diverse high-growth segments of large global markets, including consumer electronics, smart home/IoT, automotive, EVs, battery-powered appliances, network infrastructure, healthcare, and aerospace/defense.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764