Nordic’s nRF91 SiP, Now at Mouser, Offers Compact, Low-Power Cellular IoT Solution

Nya produktlanseringar

Anslut till oss


Nordic’s nRF91 SiP, Now at Mouser, Offers Compact, Low-Power Cellular IoT Solution

January 7, 2019 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the nRF91 system-in-package (SiP) from Nordic Semiconductor. Featuring an integrated application microcontroller, full LTE modem, RF front end, and power management in a single device, the nRF91 SiP is ideal for low-power cellular Internet of Things (IoT) applications.

The Nordic nRF91 SiP, available from Mouser Electronics, provides globally compatible narrowband (NB) IoT and LTE-M support in bands ranging from 700 MHz to 2.2 GHz. The device boasts an integrated Arm® Cortex®-M33 processor with Arm CryptoCell and Arm TrustZone security technology, providing secure performance in worldwide operation. The nRF9160 SiP leverages Qorvo's state-of-the-art, proven RF front-end, advanced packaging, and MicroShield™ technology to deliver a unique, ultra-compact solution that combines high performance with low power consumption. The GCF-certified, 3GPP LTE-compliant module is available with built-in GPS support, offering a cost-effective solution for asset tracking applications.

The nRF91 SiP is housed in a miniscule 10 × 16 × 1 mm package and features 32 general-purpose input and output (GPIO) pins and a broad range of peripherals and interfaces to provide a flexible solution for a wide variety smart devices. Software examples and hardware reference designs simplify the design process and significantly reduce time-to-market. The nRF91 SiP offers extended battery life and low-cost maintenance and installation, making it suitable for smart city products as well as industrial, medical, and agricultural applications.

The Nordic nRF91 SiP is supported by the nRF9160 Development Kit. The development kit enables rapid prototyping and allows access to all interfaces and IO via connectors. The nRF9160 kit features four LEDs, two switches, and two buttons, which are user-programmable for tailored performance.

To learn more, visit www.mouser.com/nordic-nrf91-series.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About Nordic Semiconductor
2026 - Nordic Semiconductor is a fabless semiconductor company specializing in wireless communication technology that powers the IoT. The company's award-winning Bluetooth Low Energy solutions pioneered ultra-low power wireless, making Nordic the global market leader. The company's development tools shield the developers from RF complexity, allowing anyone with a bright idea to build innovations based on the IoT platform. Today, Nordic's award-winning, high-performance, yet easy to design-in, Bluetooth LE, cellular IoT, and Wi-Fi solutions are used by the world's leading brands in a variety of products, including advanced wearables, smart home, medical, industrial automation, sports and fitness, logistics and transportation, etc..
Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764