Mouser Electronics Features Advanced Testing and Inventory Tools at NIWeek 2018

För omedelbar lansering

Anslut till oss


Mouser Electronics Features Advanced Testing and Inventory Tools at NIWeek 2018

May 18, 2018 - Mouser Electronics, Inc., the New Product Introduction (NPI) leader empowering innovation, will be exhibiting at NIWeek, May 21 - 24 at the Austin Convention Center. Mouser representatives will be in booth 539 to discuss the latest technology that's helping to empower innovation among design engineers.

Presented by National Instruments (NI), the 24th annual NIWeek brings together the brightest minds in engineering and science. The conference, attended by thousands of innovators, includes more than 290 interactive and hands-on sessions, targeted industry summits, and more than 100 exhibits on the latest advancements in design, research and test technology. Conference topics include 5G wireless technology, autonomous vehicles, energy, testing equipment, and data acquisition..

"We are excited to exhibit at this year's NIWeek," said Kevin Hess, Mouser Electronics' Senior Vice President of Marketing. "The event gives us an opportunity to connect with engineers from a variety of backgrounds and show them the latest technologies from top manufacturers."

Mouser will have a large presence throughout the four-day conference, hosting booth 539. Representatives will be showcasing two products from Digilent. The Digital Discovery™ module is a pocket-sized, high-performance device that combines four common bench tools to provide designers a suite of advanced features to debug, visualize and simulate digital signals for a broad array of embedded projects. The chipKIT™ Wi-FIRE™ is a Wi-Fi-enabled board based on the Arduino open source hardware platform. The board incorporates a powerful Microchip PIC32MZ microcontroller plus 43 I/Os and an onboard MRF24 wireless module.

Additionally, Mouser will be demonstrating NI VirtualBench, an all-in-one Instrument that combines a mixed-signal oscilloscope with protocol analysis, an arbitrary waveform generator, a digital multimeter (DMM), a programmable DC power supply, and digital I/O into a single device that connects to a PC or iPad. Visitors can also enter for a chance to win a set of Bose QuietComfort 35 wireless noise-cancelling headphones.

Attendees can also learn more about two robust ordering tools on Mouser.com. FORTE is Mouser's intelligent bill of materials (BOM) management tool, designed to increase confidence, save time, and improve order accuracy in specifying and purchasing electronic components. Mouser's free, easy-to-use inventory management tool and companion mobile app allow users to manage and track part numbers and inventory levels, generate inventory reports, and link products to Mouser part numbers for easy reordering.

Founded in 1976, Austin-based National Instruments is a producer of automated test equipment and virtual instrumentation software. For more information, visit www.mouser.com/national-instruments. For more information about NIWeek, visit eng.info.mouser.com/niweek-2018.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För mer information, kontakta:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
Vid pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804 7764