Improve Datacenter Throughput and Storage up to 11TB with Micron’s 9200 NVMe SSDs, Now at Mouser

Nya produktlanseringar

Anslut till oss


Improve Datacenter Throughput and Storage up to 11TB with Micron’s 9200 NVMe SSDs, Now at Mouser

April 25, 2019 - Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components, is now stocking the 9200 Series of NVM Express™ (NVMe™) solid state drives (SSDs) from Micron. One of the first NVMe SSDs on the market with a capacity exceeding 10 TB, the 9200 SSDs offer high capacity, fast speeds, and low latency for high-performance functions such as application and database acceleration, online transaction processing (OLTP), high-frequency trading, and high-performance computing.

The Micron 9200 Series SSDs, available from Mouser Electronics, blend the capabilities of 3D NAND and NVMe technologies for enterprise storage. The devices are built on an innovative architecture that combines NVMe protocols on a PCIe connection to deliver fast enterprise flash performance up to 10 times' faster than SATA SSDs, plus 3D NAND high-density storage that conserves power and rack space. The 9200 SSDs deliver sequential read/write transfer speeds up to 5.5 and 3.5 GBytes per second, with random read/write transfer speeds up to 900K and 275K input/output operations per second (IOPS) to turn data into information with low latency and high performance.

The Micron 9200 includes three endurance classes: 9200 PRO is designed for read-centric use at roughly one drive write per day (DWPD) with capacities from 1.9 TB to 7.6 TB, while the 9200 MAX supports mixed-use workloads at about three DWPD in capacities from 1.6 TB to 6.4 TB. The 9200 ECO drives offer the highest capacities at 8 TB or 11 TB and are designed for fewer than one DWPD.

The Micron 9200 SSD family is designed as the storage foundation for the Micron SolidScale™ platform, providing greater capacity for more efficient workload optimization and reducing total cost of ownership. With the 9200, SolidScale will be capable of over 250 TB per node, scaling over 5 PB per rack of one of the highest performance NVMe SSD available in shared storage today.

To learn more, visit www.mouser.com/micron-9200-nvme-ssd.

With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Micron

2026 - Micron is an industry leader in innovative memory and storage solutions, transforming how the world uses information to enrich life for all. With a relentless focus on customers, technology leadership and manufacturing and operational excellence, Micron delivers a rich portfolio of high-performance DRAM, NAND, and NOR memory and storage products through its Micron® and Crucial® brands. Every day, the innovations that Micron's people create fuel the data economy, enabling advances in artificial intelligence and 5G applications that unleash opportunities — from the data center to the intelligent edge and across the client and mobile user experience.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764