Mouser Now Shipping New Intel Quark Processor for IoT

Nya produktlanseringar

Anslut till oss


Mouser Now Shipping New Intel Quark Processor for IoT

November 3, 2015 - Mouser Electronics, Inc. is now shipping the new Intel® Quark™ microcontroller D1000, designed for Internet of Things (IoT) architectures and applications. Announced at Intel's IoT Insights event in San Francisco, along with Intel® Quark™ microcontroller D2000 and the Intel® Quark™ SE microcontroller for IoT, this new technology extends intelligent computing to a new spectrum of data actuation applications and devices that require lower power consumption. 

The Intel® QuarkTM processors are at the top of their class, designed to provide exceptional user experience through scalability across the Intel portfolio of products. The microcontroller family simplifies design and reduces bill of materials (BOM) by minimizing external components required on the platform. By developing on Intel® Quark™ technology for edge devices, solutions providers can deploy compatible software throughout the solution to tie different pieces together. 

The Intel® Quark™ microcontroller D1000, now available from Mouser Electronics, is optimized for applications that require long battery life, such as wearable sensors and RFID tags. This 32MHz, ultra-low power, 32-bit microcontroller contains 32kBytes of flash and 8kBytes of SRAM. Its comparators and analog-to-digital converters (ADCs) make it easy to connect to transducers and RF front ends, and the serial peripheral interfaces allow for seamless connection with popular sensors, radios, memories, DSPs and application processors.

The Intel® Quark™ microcontroller D2000 is an advanced version of the D1000, offering more I/O and providing ultra-low power, 32MHz, 32-bit x86 functionality. The D2000 features two PWM channels and an extended operating temperature range (-40 degrees Celsius to +85 degrees Celsius). The Intel® Quark™ SE microcontroller for IoT is a premier 32MHz, 32-bit x86 microcontroller that offers high-efficiency power consumption. It contains 384kBytes of flash and 80kBytes of SRAM, and embodies all of the features of the D2000, plus an always-listening sensor hub and pattern-matching technology. Both the D2000 and SE microcontrollers come with a full Intel x86 instruction set architecture for compatibility and scalability.

"Mouser is excited to offer the new Intel Quark processor for immediate shipping to our customers," said Russell Rasor, Mouser Electronics Vice President, Supplier Management, Advanced Technologies.

"We are pleased and proud to debut our new Intel Quark microcontrollers through Mouser Electronics," said Tanya Pelletier, senior product manager, Intel Quark Solutions Division at Intel. "We appreciate the personal attention Mouser's professionals afford both customers and manufacturers and are excited about getting this new product into the hands of design engineers."

To learn more about the Intel Quark microcontroller D1000, visit
http://www.mouser.com/new/Intel/intel-quark-d1000-mcu/.

To learn more about the Intel Quark microcontroller D2000, visit
http://www.mouser.com/new/Intel/intel-quark-d2000-mcu/.

To learn more about the Intel Quark microcontroller SE, visit
http://www.mouser.com/new/Intel/intel-quark-se-soc/.

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 21 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Intel

2026 - Intel® makes possible the most amazing experiences of the future. Many may know Intel® as the world's largest manufacturer of semiconductors, but Intel® does so much more. Intel® invents at the boundaries of technology to make amazing experiences possible for business and society, and for every person on Earth.

Harnessing the capability of the cloud, the ubiquity of the Internet of Things, the latest advances in memory and programmable solutions, and the promise of always-on 5G connectivity, Intel® is disrupting industries and solving global challenges. If it's smart and connected, it's best with Intel®.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764