Get the New Pocket-Sized Intel Compute Stick with Linux Available Now at Mouser

Nya produktlanseringar

Anslut till oss


Get the New Pocket-Sized Intel Compute Stick with Linux Available Now at Mouser

July 30, 2015 - Mouser Electronics, Inc. is now shipping the Intel® Compute Stick with Ubuntu Linux, a new generation of computer from Intel Corp. The Compute Stick is a revolutionary new device that enables any screen with an HDMI interface to become a fully functional personal computer. The Compute Stick comes pre-installed with the Ubuntu 14.04 LTS operating system. The Intel Compute Stick is a fully functional computer in a package similar to a large USB stick.

The new Intel Compute Stick with Ubuntu Linux, available from Mouser Electronics, is powered by a 64‑bit 1.33GHz Intel® AtomTM Z3735F Quad-Core processor with 2Mbytes cache, integrated Intel HD graphics, and multi‑channel digital audio. The Compute Stick plugs into any display that has an HDMI 1.4a interface. Networking is achieved with onboard IEEE 802.11 b/g/n WiFi, and peripheral connectivity is available through the Bluetooth 4.0 and USB 2.0 interfaces. Once plugged into a display's HDMI port, the user powers the Compute Stick with a wall adapter. A status LED indicates the device is powered while both graphics and audio is provided through the HDMI port. The device can be controlled through a wireless keyboard and mouse.

The Intel Compute Stick with Linux is available from Mouser Electronics running a custom build of Ubuntu 14.04 LTS operating system direct from Canonical, with all the latest updates. The stick has 8GBytes of eMMC Flash for user file storage and 1GByte of RAM. An Intel Compute Stick running Microsoft Windows 8.1 is also available from Mouser Electronics. Flash user storage is expandable for both versions through a microSDXC slot on the side of the device.

Once configured, the Intel Compute Stick has all the performance and functionality of a full-sized computer and can browse the web, view online video, edit photos and files, and play music.

To learn more, visit http://www.mouser.com/new/Intel/intel-compute-stick/.

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 21 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Intel

2026 - Intel® makes possible the most amazing experiences of the future. Many may know Intel® as the world's largest manufacturer of semiconductors, but Intel® does so much more. Intel® invents at the boundaries of technology to make amazing experiences possible for business and society, and for every person on Earth.

Harnessing the capability of the cloud, the ubiquity of the Internet of Things, the latest advances in memory and programmable solutions, and the promise of always-on 5G connectivity, Intel® is disrupting industries and solving global challenges. If it's smart and connected, it's best with Intel®.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764