Mouser Electronics Announces Global Distribution Agreement with Embedded Vision Leader FRAMOS
August 31, 2020 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, has signed a global distribution agreement with FRAMOS, a leading manufacturer of imaging and embedded vision technologies, to offer its sensor modules and processor adaptor products. Through the FRAMOS Ecosystem's expanded range of sensor modules, adapters and accessories, and development kits, vision engineers and developers can evaluate and integrate many different image sensors on open processor platforms, quickly create proofs-of-concepts, and systematically develop them further for their exact needs.
FRAMOS Sensor Modules (FSM) allow customers to seamlessly plug the latest image sensor technology into common processing platforms through the use of a fully modular design that relies on standardized connectors and mechanicals. The lineup provides an extensive range with resolutions from 0.4 MP to 24 MP that comes with rolling and global shutter options. These small modules are available from Mouser in a 26.5 mm × 26.5 mm form factor, and include native MIPI CSI-2 sensors.
FRAMOS adapters and accessories contain all the necessary periphery to operate the sensor, and transmit and convert its signals into the formats needed by the processor development boards. The FRAMOS Sensor Adapters (FSA) are stacked to the FSMs to ensure modularity and design flexibility in all application-specific designs. The FSAs include reference clocks, power rails and processing functionality with standardized connectivity for operating the imager to allow seamless interchangeability. These products provide flexibility, decrease redundancy and improve performance, and include all design documentation to support customized all-on-one-board integration. FRAMOS Processor Adaptor (FPA) boards offer a modular adaption to several third-party image processing boards within the FRAMOS EV ecosystem.
FRAMOS sensor module development kits support up to four FSMs simultaneously and include pre-assembled FSM/FSAs with a lens mount and M12 lens, tripod adapter, and all the necessary adapters for interfacing to the NVIDIA® Jetson™ hardware products and other third-party development boards. Device drivers and sample applications with source code provide a minimum environment to control the sensor and stream images directly into user applications, enabling customers to rapidly create unique applications, with little overhead. The kits also include a chainable 150 mm flex cable connecting the FSAs to the FPAs, allowing engineers to get up and running quickly with an FSM and their existing third-party processor development kit.
To learn more, visit https://www.mouser.com/manufacturer/framos/.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
2026 - FRAMOS is an imaging expert, trusted advisor, and vision solutions provider. Since 1981, FRAMOS has implemented the best current and emerging imaging technologies to address specific customer requirements and applications. FRAMOS meets these requirements with advanced and proven imaging components from a global network of renowned partners and with FRAMOS IP. More than 180 FRAMOS employees worldwide are passionate about the unlimited potential of imaging and help customers achieve the optimum results from every possible scenario. FRAMOS drives and ensures the entire product development journey from POC, through prototyping, to mass production. FRAMOS carefully selects imaging components, like image sensors, lenses, or various 3D technologies, and offers custom developments tailored to individual needs and time frames. FRAMOS listens to and understands customer challenges. With innovative solutions, FRAMOS ensures successful project outcomes and develops long-term customer relations.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.