Mouser-Sponsored Formula E Team Drives into Berlin
May 21, 2019 - Following another top-ten finish at the Monaco E-Prix, the Mouser Electronics-sponsored GEOX DRAGON Formula E racing team heads to Germany for the Berlin E-Prix on May 25. At the Monaco E-Prix, driver José María "Pechito" López continued GEOX DRAGON's successful season, coming in tenth.
Mouser is sponsoring the GEOX DRAGON Formula E team throughout the 2018-19 ABB FIA Formula E Championship racing season, in collaboration with TTI, Inc. and valued suppliers Molex and AVX. This is the fifth-straight year that Mouser and Molex have sponsored Formula E racing.
The Formula E series features cars that are powered solely by electricity and represent a vision for the future of the motor sports industry, serving as a framework for research and development around zero-emission motoring. Racing is all about speed and endurance, and racing sponsorships are an innovative way for Mouser to communicate its performance-driven business model and promote the newest technologies from its manufacturer partners.
Team drivers for the Berlin E-Prix are three-time World Touring Car Driver's Champion and multiple FIA Formula E podium finisher López and GEOX DRAGON Test and Reserve Driver, Maximilian Günther, who will take the wheel in his home country.
Fans can cast a vote for López and Günther in FANBOOST, which allows fans to play an active role in influencing the outcome of the race. FANBOOST gives fans the opportunity to vote for their favorite driver and award them an extra boost of power during the race. The five drivers with the most FANBOOST votes are awarded a significant burst of power, which they can deploy in a 5-second window during the second half of the race. FANBOOST voting for the Berlin E-Prix opened May 20 and is available up to 15 minutes into the race.
The Formula E series finishes out the Europe races in Bern, Switzerland, on June 22, before the season-ending double-header in New York, July 13 and 14.
For more information about Formula E and to register and vote in FANBOOST, visit www.mouser.com/formula-e.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
2026 - Molex believes in the transformative power of creating connections. As a leading global provider of connector solutions, Molex brings engineering excellence, trusted relationships, and an unparalleled commitment to quality and reliability to help customers across industries improve lives. Trusted for more than 80 years, Molex offers world-class design, manufacturing, and a portfolio of 100,000+ innovative products. Molex is doing more than developing solutions, it's creating connections for life.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.