Use USB Faster with the Cypress EZ USB FX3 USB 3.0 SuperSpeed Explorer Kit Available from Mouser

För omedelbar lansering

Anslut till oss


Use USB Faster with the Cypress EZ USB FX3 USB 3.0 SuperSpeed Explorer Kit Available from Mouser

February 17, 2015 - Mouser Electronics, Inc. is now stocking the EZ-USB® FX3™ USB 3.0 SuperSpeed Explorer Kit from Cypress Semiconductor. This Explorer Kit includes all the hardware, software, and documentation necessary to enable developers to evaluate the Cypress EZ-USB® FX3™, an ARM‑based USB 3.0 peripheral controller. USB 3.0 offers the SuperSpeed signaling rate of 5 Gigabits per second, ten times greater than the USB 2.0 high-speed signaling rate of 480 megabits per second.

The Cypress EZ-USB FX3 SuperSpeed Explorer Kit, available from Mouser Electronics, allows developers to add USB 3.0 SuperSpeed connectivity to any design. The development board provides convenient access to all FX3 IC interfaces. Two 40-pin headers allow the FX3 to connect to external boards using the Cypress's 2nd generation General Programming Interface (GPIF‑II). These headers use long pins that can also be used as test points. The board can connect to external devices such as FPGAs, CPLDs, image sensors, or microcontrollers. The FX3 Software Development Kit (SDK) includes example code to help learn how to program and evaluate the FX3. The SuperSpeed Explorer kit easily interfaces to Altera FPGAs as well as image sensor peripheral boards.

The USB 3.0 SuperSpeed Explorer Kit development board provides two USB connectors. The USB 3.0 Type‑B connector brings out the FX3 USB signals. This connector can accept either a USB 3.0 or USB 2.0 connector. A USB 2.0 Micro-B receptacle interfaces to an onboard Cypress CY7C65215 USB‑Serial Dual Channel UART/I2C/SPI Bridge, which is configured as the board's integrated debugger operating at the USB 2.0 Full-Speed rate. This chip provides a bridge between the FX3 debug interface and a PC's USB port, enabling serial terminal message debugging as well as JTAG debugging.

The kit also includes the Cypress EZ USB Suite, ARM GCC toolchain, FX3 firmware library, and example projects. Also included is the Cypress USB Suite and sample Microsoft Visual Studio applications. A USB 3.0 cable is included.

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser är en ledande auktoriserad distributör av elektroniska komponenter och produkter för industriell automation. Med fler än 6,8 miljoner produkter från över 1 200 varumärken erbjuder vi det bredaste urvalet av produkter i lager. Vår verksamhet inom elektroniska komponenter vänder sig till konstruktörer och inköpare med nya produktlanseringar inom halvledare, passiva komponenter, kontaktdon och relaterad elektronikteknik. Vår verksamhet inom industriell automation hjälper företag att utforma, bygga och underhålla sin tillverkningsutrustning och drift med lösningar som omfattar de senaste sensorerna, kontrollpanelerna, PLC:erna och motorstyrningarna – där allt finns i lager för omedelbar leverans.

Mouser erbjuder förstklassig kundservice med 28 kontor världen över som erbjuder support på ditt språk, i din valuta och i din tidszon. Vi levererar dagligen produkter till fler än 650 000 kunder i 223 länder och territorier från våra toppmoderna distributionsanläggningar på över 1,5 miljoner kvadratfot i storstadsområdet Dallas i Texas. Mer information finns på https://www.mouser.com.

Om Cypress Semiconductor

2026 - Cypress är ledande inom avancerade inbäddade systemlösningar för världens mest innovativa produkter inom bilindustri, industri, apparater för smarta hem, konsumentelektronik och medicin. Mikrokontrollers, analoga kretsar, trådlösa och USB-baserade anslutningslösningar samt högeffektiva minnen från Cypress hjälper konstruktörer att konstruera olika produkter och vara först på marknaden med dem. Cypress är engagerade i att förse sina kunder med den bästa supporten och de bästa utvecklingsresurserna på planeten vilket gör det möjligt för dem att störa marknader genom att skapa nya produktkategorier på rekordtid.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För mer information, kontakta:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
Vid pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804 7764