WiFi and Bluetooth Coexist with the Atmel WINC1500 Low Power WiFi Module Now at Mouser

För omedelbar lansering

Anslut till oss


WiFi and Bluetooth Coexist with the Atmel WINC1500 Low Power WiFi Module Now at Mouser

March 12, 2015 - Mouser Electronics, Inc., the global authorized distributor with the newest semiconductors and electronic components, is now shipping the new WINC1500 Wi-Fi Module from Atmel Corporation. The WINC1500 is a low-power consumption 802.11 b/g/n WiFi module specifically optimized for low power Internet of Things (IoT) applications. The WINC1500 WiFi module supports WEP, WPA, and WPA2 WiFi security encryption as well as China WAPI security while drawing as little as 4µA. This module includes features that allow both WiFi and Bluetooth signals to coexist locally without any signal interference.

The Atmel WINC1500 Wi-Fi Module, available from Mouser Electronics, is a highly integrated device featuring a small form factor at only 21.5mm x 14.5mm x3.4mm. This module includes an integrated power amplifier, low noise amplifier (LNA), all necessary power management functions, and an integrated antenna. This module targets low power WiFi wireless applications and draws only 4µA in Deep Power Down mode. When in beacon monitoring mode the module draws only 850µA in Doze Mode. This module provides SPI, UART, and I2C host interfaces for communicating with a host microcontroller. It also supports 2-wire and 3-wire Wi-Fi/Bluetooth coexistence signaling interface. The interface allows this module to coordinate transmission and reception with a compatible Bluetooth module to insure that both radios do not interfere with each other.

The Atmel WINC1500 is based on a powerful Cortus-APS3 32-bit processor. This processor performs hardware accelerated MAC functions including association, authentication, power management, security key management, and MSDU aggregation/de-aggregation. In addition, the processor provides flexibility for various modes of operation, such as STA and AP modes. An on-chip IP stack minimizes the host microcontroller requirements and supports TCP, UDP, DHCP, ARP, HTTP, SSL, and DNS.

To learn more, visit: http://www.mouser.com/new/atmel/atmel-winc1500/ .

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Atmel / Microchip

2026 - Atmel Corporation is a global leader in designing, manufacturing and marketing advanced semiconductors including microcontroller (MCU), programmable logic, and nonvolatile memory. By combining these core technologies, Atmel meets the evolving and growing needs of today's electronic system design engineer through the production of general purpose and application specific system level integrated chips. Atmel's world class expertise and wealth of experience in system-level integration enable all of Atmel's products to be developed from their constituent blocks with minimum delay and risk.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764