Amphenol Industrial Helios H4 Solar Connectors Available from Mouser

För omedelbar lansering

Anslut till oss


Amphenol Industrial Helios H4 Solar Connectors
Available from Mouser

October 27, 2014 - Mouser Electronics, Inc. is now shipping the Helios H4 Solar Connectors from Amphenol Industrial. These connectors are IP68 rated and are specifically designed to meet requirements for solar power and energy harvesting applications, boasting a very high 52 Amp rating. Helios H4 connectors provide highly efficient power transfer with extremely low loss by the use of precision machined contacts utilizing Amphenol Industrial's exclusive RADSOK® Technology.

The Amphenol Industrial Helios H4 Solar Connectors, available from Mouser Electronics, provide higher current ratings and lower contact resistance than conventional solar connector solutions. Typical contact resistance is only 0.25mΩ, resulting in extremely low power losses. Connectors mate quickly and easily with an audible snap‑lock mating system that helps insure an error-free installation. Amphenol Industrial's unique RADSOK Technology insures a high contact, low resistance connection by placing a web of about two dozen tiny beams running from the front to back of the female contact. As the male contact is inserted, the web wipes the male contact clean while providing solid multiple connections, imparting high current flow with minimal voltage loss.

These H4 Solar Connectors provide very high reliability connections and are highly resistant to the harsh environments found in solar power installations, including resistance to extremes of heat, cold, immersion in water, ozone, salt, abrasion, UV, and sunlight.

Compatible with standard industry connectors, the Helios H4 Panel Connector is available in three different gauges including 14 AWG rated at 36A, 12 AWG rated at 45A, and 10 AWG rated at 52A. These rugged connectors meet or exceed the strict standards set for solar power connectors and are compliant with UL 1000V, TUV 1500V, and CSA. These connectors also meet the new standards including NEC 2008/2011. As per NEC 2008 these connectors mate with an audible click and require a special unlock tool to unmate the connectors.

To learn more, visit: http://www.mouser.com/new/Amphenol/amphenolheliosh4/ .

With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Amphenol Industrial

2026 - Amphenol Industrial offers a wide variety of receptacles, plugs, and connectors. Amphenol Industrial has long been the accepted leader in providing quality connectors and interconnect systems to the industrial markets and is the leading manufacturer of cylindrical connectors in the world. Most Amphenol Industrial Circular Connectors are in stock or assembled and ready to ship within 7 to 10 business days.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764