Mouser Sponsors XIAO Showdown Developer Competition with Silicon Labs, Seeed Studio, and Pico Technology

För omedelbar lansering

Anslut till oss


Learn more about the XIAO Showdown Developer Competition
Learn more about the XIAO Showdown Developer Competition

August 25, 2025Mouser Electronics, Inc., the New Product Introduction (NPI) leader empowering innovation, is pleased to be a primary sponsor of the XIAO Showdown Developer Competition, along with valued manufacturer partners Silicon Labs, Seeed Studio, and Pico Technology.

The XIAO Showdown is now open. To enter the contest, participants will need to build a project using the XIAO MG24 Sense development board from Seeed Studio, then share it with the Silicon Labs Community. Silicon Labs is also giving away free hardware to enable contestants to jumpstart their build. The first 20 people who submit an eligible project idea will receive a free XIAO MG24 Sense development board shipped straight to them. To qualify, contestants will need to explain their project, using the form provided on the XIAO Showdown site. The project doesn't have to be finished or even started, but contestants must provide thoughtful ideas that fit the contest criteria.

Seeed Studio's XIAO MG24 Sense development board is based on the Silicon Labs EFR32MG24 system-on-chip (SoC) featuring a high-performance 78MHz Arm® Cortex®-M33 core. The XIAO MG24 Sense is Matter® native over Thread® and Bluetooth® Low Energy 5.3, all supported by the Arduino® Core. The development board also features 4MB Flash, 19 GPIOs, and an onboard charging circuit. Its low operating currents and ultra-low-power modes make it an ideal choice for Internet of Things (IoT) applications, especially battery-powered projects utilizing Matter protocols.

The grand prize winner will receive a $500 gift certificate from Mouser.com, a $1,000 coupon for Seeed Studio Fusion PCBA, a PicoScope 3203D, and more. Second and third place winners will also receive coupons from Seeed Studio Fusion PCBA and benchtop oscilloscopes from Pico Technology.

To view the full list of prizes and contest rules, submit a project idea, and register for the XIAO Showdown Developer Competition, visit https://get.silabs.com/XiaoShowdown/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764