Mouser-Sponsored Vasser Sullivan Lexus Racing Team Celebrates Double Podium at IMSA Long Beach

Mouser and Molex Sponsor Team Throughout 2022 IMSA Championship Season
För omedelbar lansering

Anslut till oss


April 12, 2022 – The Mouser Electronics-sponsored Vasser Sullivan Lexus Racing team is celebrating a spectacular double-podium finish at the Acura Grand Prix of Long Beach (California) this past weekend. Jack Hawksworth and Ben Barnicoat piloted the No. 14 Vasser Sullivan Lexus RC F GT3 to a second-place finish in GTD PRO Class, while Frankie Montecalvo and Aaron Telitz in the No. 12 car finished third in the GTD Class.

“Congratulations to the Vasser Sullivan Lexus team on their double-podium wins at Long Beach. From the pit to the drivers’ seats, the team came together to deliver an exciting race with awesome results!” said Todd McAtee, Mouser’s Vice President of Americas Business Development. “This season gets more exciting with every race, and Mouser and Molex are proud to support the Vasser Sullivan Lexus team’s first-class program.”

Mouser, the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is teaming up with Molex LLC to sponsor both the No. 14 Vasser Sullivan Lexus RC F GT3 GTD PRO Class and the No. 12 Vasser Sullivan Lexus RC F GT3 GTD Class entries for the 2022 IMSA WeatherTech SportsCar Championship season. Team drivers for the season include Jack Hawksworth, Kyle Kirkwood and Ben Barnicoat in the No. 14 car and Townsend Bell, Richard Heistand, Frank Montecalvo and Aaron Telitz in the No. 12 car.

Mouser previously sponsored the Vasser Sullivan IndyCar team, seeing the opportunity as an inventive way to communicate its performance-driven business model and promote the newest technologies; since then, the Mouser and Molex relationship with Vasser Sullivan has bred success, having won the Indianapolis 500 and producing multiple wins and podiums with Vasser Sullivan IndyCar.

The 2022 season will mark the fourth season Lexus and Vasser Sullivan have partnered together. During that time, the Lexus RC F GT3 has earned seven GTD class wins, 18 podiums and nine pole positions.

The season continues April 29 at the Hyundai Monterey Sports Car Championship at Laguna Seca, California, followed by seven more races before the finale at Motul Petit Le Mans, September 28–October 1 in Atlanta.

For more about the Mouser-sponsored Vasser Sullivan Lexus Racing team, visit https://www.mouser.com/imsa-racing/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764