Mouser Electronics and Molex Gear Up to Support Vasser Sullivan Lexus Racing for 2025 IMSA Season

För omedelbar lansering

Anslut till oss


January 14, 2025Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, today announced its continued associate sponsorship of the Vasser Sullivan Lexus Racing team for the 2025 IMSA WeatherTech SportsCar Championship Series.

Mouser is teaming up again with valued manufacturer partner Molex to sponsor the No. 14 Vasser Sullivan Lexus RC F GT3 GTD PRO and the No. 12 Vasser Sullivan Lexus RC F GT3 GTD Class entries for the 2025 IMSA season. The season kicks off January 17-19 with the Roar Before the Rolex at Daytona International Speedway in Florida, followed by the 2025 Rolex 24 at Daytona, January 23-26.

"For more than ten years, together with Molex, we've supported high-performance motorsports and are super excited to continue our sponsorship of Vasser Sullivan Lexus Racing in the 2025 IMSA series," said Todd McAtee, Senior Vice President, Business Development for Mouser Electronics. "Mouser is honored to be part of this team's first-class racing program."

The full-time driver lineups for Vasser Sullivan Racing include Ben Barnicoat and Aaron Telitz in the No. 14 Lexus RC F GT3 in the GTD PRO class, with Jack Hawksworth and Parker Thompson co-driving the No. 12 Lexus entry in the GTD class. Kyle Kirkwood and Frankie Montecalvo join the driver pairs in the No. 14 and 12 cars for select IMSA WeatherTech SportsCar Championship endurance races this season. The team will look to continue the momentum of 2024, where they ended the season with two wins, four podium results and five pole positions. Parker Thompson led the GTD class with three poles.

Mouser previously sponsored the Vasser Sullivan IndyCar team, seeing the opportunity as an inventive way to communicate its performance-driven business model and promote the newest technologies. Since then, the Mouser and Molex relationship with Vasser Sullivan has resulted in many successes, winning the Indianapolis 500 in 2013 and producing multiple wins and podiums with Vasser Sullivan IndyCar and now Vasser Sullivan Lexus Racing.

For more information on Mouser's sponsorship of the Vasser Sullivan Lexus racing team and to see the schedule for the 2025 season, visit https://www.mouser.com/imsa-racing/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764