New eBook from STMicroelectronics and Mouser Explores Future of Responsive AI at the Edge

För omedelbar lansering

Anslut till oss


October 25, 2022Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, announces a new eBook in collaboration with STMicroelectronics (ST), exploring the development of artificial intelligence (AI) and machine learning (ML) at the edge. In Intelligence at the Edge, subject matter experts from Mouser and ST offer deep analyses of the challenges and applications for AI and ML development at the edge. The eBook features articles on topics such as intelligent sensors, embedded neural networks, and responsive AI.

AI-driven technology and devices will eventually transform the ways in which we live and work, leading to increase productivity, enhanced quality of life, and greater environmental sustainability. However, cloud AI applications demand tremendous resources in terms of power, bandwidth, and data, while also posing important questions regarding privacy and security. As AI migrates from cloud servers to the network edge, machine learning models deployed on embedded microcontrollers will facilitate a dramatic expansion in AI-backed applications and devices. The new eBook features a range of articles, infographics, and instructional videos to explain the potential use of ST products in edge-AI applications.

Intelligence at the Edge offers direct links to more than a dozen relevant solutions from ST. Featured products include the STM32U5 series of ultra-low-power microcontrollers for advanced applications, including wearable devices, industrial sensors, home automation, and personal medical devices. The microcontrollers are based on an Arm® Cortex®-M33 core and offer 2 Mbytes of flash memory and 786 Kbytes of SRAM. ST’s NanoEdge™ AI Studio allows developers to quickly create optimal AI libraries for specific projects without requiring data science skills or knowledge. The NanoEdge AI Studio helps developers to easily detect security concerns and conduct predictive maintenance.

ST solutions available from Mouser include microcontrollers, sensor kits, power management ICs, and memory devices. To learn more about STMicroelectronics, visit https://www.mouser.com/manufacturer/stmicroelectronics/. To read the new eBook, go to https://www.mouser.com/news/st-intelligenceattheedge-infographic/st-intelligenceattheedge-ebook.html.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om STMicroelectronics

2026 - STMicroelectronics is a global independent semiconductor company and a leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivaled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio, and strategic partners positions, STMicroelectronics is at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence trends.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764