Mouser and STMicroelectronics Develop New Content Stream Devoted to the Latest in Industry 4.0

För omedelbar lansering

Anslut till oss


September 21, 2021Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, and STMicroelectronics (ST), a global semiconductor leader serving customers across the spectrum of electronics applications, have partnered to create a new resource site highlighting the products, insights and strategies required for smart industry designs. Designers and engineers can access the platform by visiting https://st.mouser.com/industry-4-0.

STMicroelectronics is a technology leader in enabling designs for Industry 4.0, offering the connectivity and sensor solutions needed to create the next generation of smart designs. The new Industry 4.0 content stream includes more than two dozen articles, flipbooks, and product descriptions to support advanced industrial solutions.

The site also features Industrial Sensing Solutions, a recent eBook from Mouser and ST that explores the different types of intelligent sensors and the technical challenges that may arise when using them in designs. Each article and flipbook includes product information for relevant STMicroelectronics products, allowing engineers to quickly identify and learn about the technology needed for Industry 4.0 applications.

Mouser offers a wide range of ST solutions, including several sensors and development kits for prototyping intelligent industrial applications. STEVAL-MKSBOX1V1 SensorTile.box is a ready-to-use development kit with wireless Internet of Things (IoT) and wearable sensor platform to help engineers use and develop apps based on remote motion and environmental sensor data, regardless of expertise level. ST’s STEVAL-BFA001V2B industrial reference design kit makes it easy for engineers to build condition monitoring and predictive maintenance solutions for industrial applications. The easy-to-use kit includes a specialty industrial sensor board as well as a programming and debugging tool.

To learn more about STMicroelectronics, visit https://www.mouser.com/manufacturer/stmicroelectronics/.

To visit the Industry 4.0 content stream, go to https://st.mouser.com/industry-4-0.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om STMicroelectronics

2026 - STMicroelectronics is a global independent semiconductor company and a leader in developing and delivering semiconductor solutions across the spectrum of microelectronics applications. An unrivaled combination of silicon and system expertise, manufacturing strength, Intellectual Property (IP) portfolio, and strategic partners positions, STMicroelectronics is at the forefront of System-on-Chip (SoC) technology and its products play a key role in enabling today's convergence trends.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764