Mouser Electronics, in Collaboration with STMicroelectronics, Explores Wireless Connectivity in New eBook

För omedelbar lansering

Anslut till oss


June 3, 2024Mouser Electronics, Inc., the New Product Introduction (NPI) leader empowering innovation, today announces a new eBook in collaboration with STMicroelectronics, offering an in-depth look at wireless connectivity.

The plethora of new and pre-existing connected Internet of Things (IoT) and Industrial Internet of Things (IIoT) devices, gateways, and sensors require that wireless technology be dependable and compatible with many wireless protocols. This need will only grow as more technologies, such as connected vehicles, medical and wearable devices, and wireless charging fully mature. In Beyond the Wires: Exploring Bluetooth and LoRaWAN Connectivity, experts from STMicroelectronics discuss the evolution of the Bluetooth® Low Energy and LoRaWAN wireless standards and their benefits.

The eBook offers many use cases, from remote sensor networks to smart cities and homes, from agriculture to public entertainment. Special requirements for security, private networks, long-range and more are also discussed. The eBook also highlights relevant products from STMicroelectronics, including the company's industry-leading RF system-on-chip (SoC) solutions, modules and development tools.

The STM32WBA5 multiprotocol wireless radio microcontroller (MCU), available from Mouser, features a powerful Arm® Cortex®-M33 core and is certified for the Bluetooth Low Energy 5.4 protocol, Zigbee® R23 and OpenThread® 1.3. The STM32WBA5 offers an ultra-low-power platform and inherited digital/analog peripherals, suitable for many applications, from industrial to smart home and consumer markets.

The STM32WLE5 wireless long-range microcontroller embeds a powerful and ultra-low-power LPWAN radio solution consisting of LoRa®, (G)FSK, (G)MSK, and BPSK. The Arm core of this MCU implements a full set of DSP instructions and an independent memory protection unit (MPU) that enhances application security.

The NUCLEO-WBA55CG Nucleo-64 board eases prototyping applications with the STM32WBA5 wireless microcontroller. Arduino Uno V3 connectivity support and ST morpho headers allow functionality expansion with a wide choice of specialized shields.

The STEVAL-ASTRA1B evaluation board includes LoRa, Bluetooth LE, and NFC, as well as a GNSS positioning module and MEMS sensors (including temperature and pressure sensors, an accelerometer, and a gyroscope), making it a complete proof-of-concept for asset tracking and monitoring.

The STEVAL-PROTEUS1 evaluation board includes Bluetooth LE, MEMS sensors and secure elements to target Industry 4.0 applications with condition-based maintenance and predictive maintenance, including the capability of anomaly detection thanks to AI capability.

The STM32WBA55G-DK1 Discovery kit is a complete demonstration and development platform for the STM32WBA55CGU7 MCU, enabling a wide diversity of applications by exploiting low-power communication, the Bluetooth SIG isochronous channel feature related to audio capability for Bluetooth Low Energy Audio, Matter as Border Router, and Zigbee.

To learn more about STMicroelectronics, visit https://www.mouser.com/manufacturer/stmicroelectronics/. To read the new eBook, visit https://resources.mouser.com/manufacturer-ebooks/st-beyond-the-wires-bluetooth-lorawan-connectivity/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764