SparkFun XBee Development Boards, Now at Mouser, Enable Rapid Prototyping with Digi XBee 3 Modules for LTE IoT Applications
February 21, 2024 – Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the XBee® development boards from SparkFun. Designed to work with the XBee 3 Global LTE-M/NB-IoT and XBee 3 Global LTE GNSS Cat 1 smart modems by Digi, these development boards enable designers to quickly integrate cutting-edge LTE cellular into their devices and applications, eliminating the time-consuming and expensive FCC and carrier end-device certification process.
The SparkFun XBee development boards are designed to help users quickly and easily prototype low-power cellular IoT applications using the new XBee 3 Global LTE-M/NB-IoT and XBee 3 Global LTE GNSS Cat 1 smart modems, also available from Mouser. These boards break out all the functionality of the XBee modules and provide the ability to connect to the cellular network and GNSS.
The XBee development boards include Qwiic connectors for I2C-capable sensors and peripherals, allowing users to quickly develop connected sensor applications. Most of the boards also include USB Type-C™ connectors for UART communication and firmware updates. While the development boards are specifically designed for the XBee 3 smart modem modules, they are also backward compatible with most previous through-hole Digi XBee modules.
Digi Remote Manager® allows users to easily configure and control devices from a central platform. Built-in Digi TrustFence® security, identity, and data privacy features use multiple layers of control to protect against new and evolving cyber threats. Standard XBee API frames and AT commands, MicroPython, and XCTU® simplify setup, configuration, testing and adding or changing functionality.
Also available is the SparkFun KIT-24441 Digi XBee kit, which includes an XBee development board, the XBee 3 Global LTE-M/NB-IoT smart modem, a humidity sensor breakout board, an LTE wide band flex antenna, and a Hologram eUICC SIM card.
To learn more about the SparkFun XBee development boards, visit https://www.mouser.com/new/sparkfun/sparkfun-xbee-development-boards/.
To learn more about the Digi XBee 3 Global LTE-M/NB-IoT smart modem, visit https://www.mouser.com/new/digi-international/digi-xbee-3-global-lte-smart-modems/.
To learn more about the Digi XBee 3 Global GNSS LTE CAT 1 smart modem, visit https://www.mouser.com/new/digi-international/digi-xbee-3-global-gnss-modems/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
2026 - As a manufacturer and proponent of open-source hardware, SparkFun has been helping turn ideas into reality since 2003. Whether you’re creating a smart weather station, exploring the frontier of machine learning, or prototyping a product, SparkFun’s ever-growing catalog has the products and resources you need to start something.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.