Mouser Electronics Offers Latest in Autonomous Vehicle Design Resources for Engineers

För omedelbar lansering

Anslut till oss


May 23, 2023Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is helping engineers stay ahead of the latest automotive design trends with an extensive content hub dedicated to resources and developments in autonomous vehicle technology. With increasingly complex hardware and systems, these vehicles require reliable, connected solutions to create a seamless user experience. Driver safety, whether on the road or via cybersecurity, requires significant consideration, making it all the more critical for automotive designers to have access to trustworthy resources and made-to-order components.

Mouser provides technical resources for various automotive design aspects, such as LiDAR design and ADAS power, in the all-inclusive content hub. Access to Mouser's articles, videos, and blogs enables designers of all skill levels to find advanced solutions with reputable components.

Mouser stocks the industry's widest selection of semiconductors and electronic components, including the following solutions for autonomous vehicle applications:

  • u-blox SAM-M10Q Standard Precision GNSS Antenna Module is a small, high-performance module with a simple interface that enables easy incorporation into user designs. The low power consumption allows for greater power autonomy for battery-operated devices. This device offers excellent out-band jamming immunity, such as caused by mobile phones. The SAM-M10Q also detects jamming and spoofing attempts and reports them to the host, so the system can react to such events.
  • ams OSRAM SPL SxL90A LiDAR QFN Packaged SMT Lasers allow autonomous vehicles to "see" farther and more effectively with the infrared LiDAR components. These devices feature low-thermal resistance to withstand temperatures at high currents. These lasers are specially made for industrial automation, 3D sensing and more.
  • STMicroelectronics SPC58 N Line Performance Microcontrollers are built to perform at high speeds with three cores that process accurately in real time. Meeting the highest ASIL-D safety levels, these microcontrollers are ideal for various automotive applications, such as powertrains, Hybrid Electric Vehicles, and ADAS. These devices support high operating temperatures and ensure augmented connectivity through different communication interfaces.
  • Taoglas Raptor III MA1280 7-in-1 Public Safety Antenna is mounted in a small, robust, IP67-rated enclosure. The antenna is suitable for all automotive and commercial trucking applications and can be modified for use at different frequencies. It features multiband GNSS (GPS/GLONASS/BeiDou/Galileo), two 5G/4G cellular MIMOs, two dual-band Wi-Fi®, active AM/FM, and LMR (700 MHz to 900 MHz) antennas.

For the latest on solutions for autonomous vehicles, visit https://resources.mouser.com/autonomous/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764