Mouser Electronics Spotlights Latest Offerings from Skyworks Solutions, Inc.

Nya produktlanseringar

Anslut till oss


November 9, 2023Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is stocking the latest innovations from Skyworks Solutions, Inc., a leading manufacturer and supplier of high-performance analog and mixed-signal semiconductors for aerospace, automotive, broadband, smartphone, cellular infrastructure, industrial, connected home and medical applications. Partnering since 2012, Mouser continues to expand its customers' product development process by offering more than 55,000 parts from Skyworks, one of the most extensive product portfolios in the industry, providing world-class solutions for customers in virtually all industries.

Mouser's inventory includes the latest Skyworks offerings:

  • The SKY55951-11 front-end module (FEM) is suitable for Global Navigation Satellite System (GNSS) receiver applications. It features an integrated L1 low-noise amplifier (LNA) and post-filter, along with an L5 LNA and post-filter. Part of the Sky5® portfolio, the SKY55951-11 provides high gain, low current consumption, and integrated input and output matching for L1 and L5, all in a compact package.
  • The OLC449 is a radiation-tolerant phototransistor, non-hermetic surface-mount optocoupler useful for satellite constellation, surveillance, avionic, and radar applications. The optocoupler consists of an LED and N-P-N silicon phototransistor that is electrically isolated but optically coupled inside a non-hermetic six-pin leadless chip-carrier (LCC) package. This optocoupler offers a low LED operating current while providing excellent radiation tolerance margins.
  • The SI83004 and SI83014 smart switches are excellent choices for driving resistive and inductive loads like solenoids, relays, and lamps commonly found in industrial control systems like programmable logic controllers (PLC). The versatile switches can be interfaced directly with an MCU or controlled through a digital isolator or optocoupler-based isolation barrier. The devices have a logic interface that supports low-power 2.5 V to 5 V microcontrollers and is powered by the switch's high-voltage field power supply.
  • Skyworks' SI86Sx digital isolators are low-power CMOS devices offering substantial data rate (150 Mbps), propagation delay (10 ns), power, size, reliability, and external BOM advantages over legacy isolation technologies. Automotive Grade options are available for specific part numbers; those Automotive Grade devices are built using automotive-specific flows in the manufacturing process intended to address the robustness and low defectivity needed in such applications.

To learn more about the wide selection of Skyworks Solutions products available from Mouser Electronics, visit https://www.mouser.com/manufacturer/skyworks-solutions/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About Skyworks Solutions Inc.

2026 - Skyworks Solutions, Inc. is empowering the wireless networking revolution. The company's highly innovative analog and mixed-signal semiconductors are connecting people, places and things spanning a number of new and previously unimagined applications within the aerospace, automotive, broadband, cellular infrastructure, connected home, defense, entertainment and gaming, industrial, medical, smartphone, tablet, and wearable markets. Skyworks is a global company with engineering, marketing, operations, sales, and support facilities located throughout Asia, Europe and North America. Skyworks and Sky5 are trademarks or registered trademarks of Skyworks Solutions, Inc. in the United States and other countries.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764