Now at Mouser: Silicon Labs' EFR32xG24 Channel-Sounding Pro Kit for Developing Bluetooth Channel Sound Products

Nya produktlanseringar

Anslut till oss


April 7, 2025Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the EFR32xG24 channel-sounding pro kit from Silicon Labs. With the EFR32xG24 kit, developers can quickly create and prototype products that use channel sounding to measure the distance between Bluetooth-connected devices. Channel sounding is used in applications such as smart home locks, phone locators, pet trackers, and industrial and commercial Internet of Things (IoT) solutions such as geofencing and access control.

The Silicon Labs EFR32xG24 channel-sounding pro kit, now available at Mouser, provides a complete reference design for the EFR32xG24 wireless system-on-chips (SoCs). The Pro Kit includes two wireless pro kit mainboards, two dipole antennas, and two radio boards. Additional features include an advanced energy monitor (AEM), packet trace interface (PTI), a virtual COM port, and a SEGGER J-link onboard debugger. For reliable performance across applications, the EFR32xG24 channel-sounding pro kit offers Ethernet and USB connectivity and a Silicon Labs relative humidity and temperature sensor. Channel Sounding is a new protocol stack for accurately measuring the distance between two Bluetooth Low Energy (LE) connected devices. The devices, one the initiator and the other the reflector, exchange information across 72 RF physical channels — the initiator transmits, and the reflector responds. The two devices then exchange packets and calculate the distance between them based on the time it took for the packets to travel back and forth.

The product's channel sounding's cross-verification process helps detect anomalies to ensure applications are secure, which is critical when developing access control solutions for hospitals and industrial buildings. Bluetooth Channel Sounding uses Phase-Based Ranging (PBR), Round Trip Time (RTT), or both for accurate coordination across the 2.4 GHz spectrum.

To learn more, visit https://www.mouser.com/new/silicon-labs/silicon-labs-xg24-pk6036a-pro-kit/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About Silicon Labs

2026 - Silicon Labs is a leading innovator in low-power wireless connectivity, building embedded technology that connects devices and improves lives.  Merging cutting-edge technology into the world’s most highly integrated SoCs, Silicon Labs provides device makers with the solutions, support, and ecosystems needed to create advanced edge connectivity applications. Headquartered in Austin, Texas, Silicon Labs has operations in over 16 countries and is the trusted partner for innovative solutions in the smart home, industrial IoT, and smart cities markets.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764