Mouser Electronics Partners with Siemens on Distribution Agreement for Industrial Automation Solutions

För omedelbar lansering

Anslut till oss


October 30, 2023Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, today announces a distribution agreement with Siemens, a world leader in industrial automation. Siemens' operations encompass factory automation and digitalization in the process and manufacturing industries, intelligent infrastructure for buildings and distributed energy systems, rail transport solutions, as well as health technology and digital healthcare services. Mouser will be stocking parts from Siemens in a variety of product categories, including networking devices, human-machine interface (HMI) solutions, circuit protection and power supplies.

"Mouser is very pleased to add Siemens to our list of trusted supplier partners. They are a world-renowned leader of industrial automation solutions, and we're excited to offer their innovative products, technologies and services to our line card for customers," said Jeff Newell, Senior Vice President of Products for Mouser Electronics. "We look forward to a successful, long-term partnership."

"Adding Mouser Electronics as a channel partner positions Siemens to better support our customers and enhance our worldwide distribution network," said James Washburn, Vice President and Segment Head Circuit Protection and Controls at Siemens. "We'll be able to satisfy more of the requirements of our existing customers, and, leveraging Mouser's excellent design and supply-chain services and logistics support, we can drive new growth opportunities, expand our presence and get our products into the hands of engineers and buyers even faster."

Mouser now offers Siemens' industrial automation products, such as the SIRIUS 2 contactors, which provide high contact reliability, prolonged endurance and usability in extreme conditions. The SIRIUS 2 contactors feature a modular design and a high performance-to-size ratio, saving valuable control cabinet space.

Also available from Mouser, the Siemens SIRIUS ACT series offers a unique portfolio of elegantly designed push buttons, indicator lights and switches that perfectly embody style, intelligence, and physical toughness. Constructed with genuine metal and high-grade plastics and engineered with smart functions and communication capabilities, these push buttons, indicator lights and switches have been element-tested to ensure reliability for mission-critical operations.

Siemens SITOP PSU100C power supplies feature a space-saving slim design and are suitable for distributed applications in control boxes or small control cabinets. The SITOP PSU100C power supplies are characterized by their low power loss over the entire load range. Power loss is extremely low even during no-load operation, making them ideal for machinery and equipment that is often in standby mode.

The LOGO! logic modules are programmable logic controllers (PLCs) that enable quick implementation of automation projects. Using the LOGO! modules, designers can quickly implement functions, such as timer switch, timer relay, counter, and auxiliary relay. Their compact, modular design saves cabinet space and allows for easy integration.

To learn more about Siemens, visit https://www.mouser.com/manufacturer/siemens/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Siemens

2026 - Siemens focuses on industry, transport, infrastructure, and healthcare and creates technology with purpose by adding real value for customers. Combining the real and digital worlds, this company empowers engineers to transform their industries and markets.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764