Mouser Electronics and Sensirion Host Webinar on Air Quality and Flow Sensing in HVAC

För omedelbar lansering

Anslut till oss


Register for the Webinar
Register for the Webinar

February 23, 2026Mouser Electronics, the authorised global distributor with the newest semiconductors and electronic components, has teamed up with Sensirion to present a new technical webinar for engineers titled "What to Know About Smart Air Quality & Flow Sensing in HVAC." The free-to-attend webinar will take place on 17th March 2026 at 17:00 CET.

As global building regulations place increasing emphasis on energy efficiency, indoor air quality (IAQ), and sustainability, HVAC system design is evolving beyond traditional demand control volume (DCV) and variable air volume (VAV) ventilation approaches. Engineers are increasingly required to balance tighter energy budgets with stricter air quality expectations, while also aligning with regional and international standards and green building frameworks. In this webinar, engineers will gain a clearer understanding of how advanced sensing supports modern HVAC design under these regulatory and performance requirements.

This expert-led webinar will address:

  • The role of next-generation sensing technologies in enabling intelligent and standards-aligned ventilation systems beyond basic CO₂ monitoring.
  • Factors driving the adoption of advanced air cleaning and energy recovery ventilation, including ASHRAE 62.1 IAQP-based approaches, filtration strategies, and the increasing importance of airflow and humidity measurement.
  • How regulatory and market trends in Europe and North America are influencing HVAC system design, and how sensor technologies support improved IAQ and energy performance in heat recovery ventilation (HRV) and energy recovery ventilation (ERV) systems.

The webinar will provide practical insight using examples of Sensirion sensing technologies, including:

  • SCD43 CO₂ Sensor Evaluation Kit – a development kit featuring the SCD43 high-accuracy photoacoustic NDIR CO₂ sensor on a reference board, enabling rapid evaluation and prototyping for indoor air quality monitoring, HVAC, and industrial process applications.
  • STCC4 Miniature CO₂ Sensor – an ultra-compact, factory-calibrated CO₂ sensor that supports integration into space-constrained designs, enabling reliable CO₂ measurement with low power consumption and suitable for applications such as indoor air quality monitors, air conditioners, smart thermostats, and other compact HVAC and building automation devices.
  • SDP3x Differential Pressure Sensor – compact differential pressure sensors based on Sensirion's CMOSens® technology, offering high accuracy and long-term stability with no zero-point drift, suitable for applications including HVAC, appliances, medical devices, and drones.

The session will be hosted by Stuart Cording, The Electronics Reporter, an engineer turned influencer with 25 years' experience in semiconductors and embedded systems, and will feature two guest speakers from Sensirion: Christian Ebneter, Senior Global Market Manager HVAC and Appliance, and Dr. Kaitlin Howell, Senior Product Manager for CO₂ Gas Sensing.

To register for live attendance or access to the on-demand recording when available, visit https://emea.info.mouser.com/sensirion-greenbuildingwebinar-event-emea-emeaen/.

To learn more about Sensirion, visit https://www.mouser.com/manufacturer/sensirion/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About Sensirion

2026 - Sensirion is a leading sensor manufacturer, providing relative humidity sensors and flow sensor solutions with unique performance. The company's product range includes liquid flow sensors, mass flow meters, mass flow controllers and differential pressure sensors. Using Sensirion's microsensor solutions, OEM customers benefit from the proven CMOSens® technology and excellent technical support. Among a large variety of applications, flow and humidity sensors are successfully used in the automotive and medical industries.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För pressförfrågningar, kontakta:
Janice Fenton
Direktör för B2B-kundansvar med ansvar för originalitetsverifiering
+44 (0) 7984 077330
För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833