Mouser Provides Design Engineers with Digital Defense Knowledge in Online Security Resource Center

Nya produktlanseringar

Anslut till oss


Visit Mouser's online security resource center.
Visit Mouser's online security resource center.

August 28, 2025Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, equips electronic design engineers with the latest cybersecurity and product knowledge in its comprehensive security resource center. As technology advances, so do the methods of cybercriminals, demanding innovative and adaptable defense strategies. Two prominent and increasingly complex issues in today's landscape are the rise of generative AI phishing and the rapid growth of the Internet of Things (IoT). These challenges emphasize the need for both technological solutions and heightened human awareness to ensure digital safety. To visit the online resource center, go to https://resources.mouser.com/security/.

The field of cybersecurity has quickly evolved in response to the increasing sophistication of digital threats. Generative AI, for instance, is reshaping the phishing landscape by creating personalized, grammatically accurate, and contextually relevant attacks at scale. At the same time, the rapid deployment of IoT devices often leads to limited processing power, infrequent patch cycles, and suboptimal security configurations, leaving many devices and connected systems unprotected. Addressing these vulnerabilities requires a rigorous approach to IoT defense measures and component selection. These potential threats highlight the critical importance of modern cybersecurity models like zero-trust architecture. This approach requires verification for all access requests, taking into account identity, contextual factors, and real-time risk assessments.

Mouser stocks the industry's widest selection of semiconductors and electronic components, including the following products and solutions for security applications:

The STM32N6 high-performance microcontrollers from STMicroelectronics are powered by the Arm® Cortex®-M55, running at 800MHz. These MCUs introduce Arm Helium™ vector processing for DSP capabilities and feature the ST Neural-ART accelerator™, an in-house NPU designed for power-efficient edge AI applications. The MCUs support real-time neural network inference for computer vision and audio tasks, making them ideal for automotive, smart home, and personal healthcare applications.

The AR0145CS Hyperlux™ SG image sensors by onsemi are 1/4.3" CMOS digital image sensors with an active-pixel array of 1280 (H) x 800 (V). They incorporate an innovative global shutter pixel design optimized for accurate and fast capture of moving scenes. The AR0145CS produces extraordinarily clear, sharp digital pictures and can capture both continuous video and single frames, which makes the sensors the perfect choice for a wide range of applications, including scanning and industrial inspection.

The S2GO SECURITY OPTIGA™ Trust X Shield2Go board by Infineon Technologies is a "plug and play" prototyping board featuring the OPTIGA Trust X security controller. This turnkey security solution for industrial automation, smart homes, and consumer devices protects authenticity, integrity, and confidentiality through mutual authentication, secured communication, data store protection, and platform integrity protection.

The EdgeLock A5000 Secure Authenticator from NXP Semiconductors offers Common Criteria EAL 6+ certified security, with symmetric and asymmetric crypto. The A5000 is used for simple authentication, complementing NXP's EdgeLock secure element family portfolio. It is an optimized and dedicated authentication product, making it ideal for battery systems, medical, and smart home applications.

Mouser's resource content hub features comprehensive articles, blogs, eBooks, and products from Mouser's technical team and trusted manufacturing partners. In a recent eBook with NXP, 7 Experts Discuss Managing Security Risk and Regulatory Compliance at the Edge, security risk management and regulatory compliance are explained in depth to provide practical guidance on implementing defense strategies. Engineers can utilize the hub as a valuable resource to keep pace with the changing world of cybersecurity threats and ensure technological protection.

To learn more, visit https://resources.mouser.com/security/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser är en ledande auktoriserad distributör av elektroniska komponenter och produkter för industriell automation. Med fler än 6,8 miljoner produkter från över 1 200 varumärken erbjuder vi det bredaste urvalet av produkter i lager. Vår verksamhet inom elektroniska komponenter vänder sig till konstruktörer och inköpare med nya produktlanseringar inom halvledare, passiva komponenter, kontaktdon och relaterad elektronikteknik. Vår verksamhet inom industriell automation hjälper företag att utforma, bygga och underhålla sin tillverkningsutrustning och drift med lösningar som omfattar de senaste sensorerna, kontrollpanelerna, PLC:erna och motorstyrningarna – där allt finns i lager för omedelbar leverans.

Mouser erbjuder förstklassig kundservice med 28 kontor världen över som erbjuder support på ditt språk, i din valuta och i din tidszon. Vi levererar dagligen produkter till fler än 650 000 kunder i 223 länder och territorier från våra toppmoderna distributionsanläggningar på över 1,5 miljoner kvadratfot i storstadsområdet Dallas i Texas. Mer information finns på https://www.mouser.com.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För mer information, kontakta:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
Vid pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804 7764