Mouser Completes SOC2 Type2, ISO 27001 Stage 2, and Cyber Essentials Certifications, Reinforcing Its Commitment to Data Security

För omedelbar lansering

Anslut till oss


December 11, 2023Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, today announces its successful completion of its System and Organization Controls 2 Type II (SOC 2 Type II), along with also receiving ISO 27001 and Cyber Essentials certification. Mouser’s customers can trust that it has the rigorous processes in place to protect the security, privacy and availability of its data, systems and products, which are 100% authorized from over 1,200 manufacturers of semiconductors and electronic components.

Following the highest data security standards, Mouser is dedicated to managing cyber security and minimizing risks through its comprehensive Information Security Management System (ISMS). Registration to these gold standards lets customers and manufacturers know that Mouser is fully committed to protecting their information.

"Mouser's SOC2 Type2, ISO 27001 Stage 2, and Cyber Essentials certifications are a testament to our unwavering commitment to security and compliance," said Raju Shah, Senior Vice President of Information Services at Mouser Electronics. "We are excited to have met and surpassed these standards, and we will continue to invest in the best practices and technologies to ensure the safety of our customers' and manufacturers' data."

SOC2, ISO 27001 and Cyber Essentials are a set of domestic and international standards that support the requirements for an ISMS. This framework helps organizations manage their cyber security risks and includes policies, processes, and controls designed to protect information assets from threats.

To be certified in these frameworks, Mouser had to meet all rigorous requirements laid out in the standards. This includes developing and implementing an information security policy, establishing risk management processes, identifying risks, implementing controls to mitigate risks, and more measures.

Mouser achieved these certifications through five independent assessments in 2023 and will undergo periodic reassessments to maintain these top certifications.

To learn more, visit https://www.mouser.com/trust/.

To view Mouser’s privacy policy, visit https://www.mouser.com/privacypolicy/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För mer information, kontakta:
Kevin Hess, Mouser
Senior Vice President of Marketing
+1 (817) 804-3833
Vid pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser
Manager, Corporate Communications and Media Relations
+1 (817) 804 7764