Mouser Highlights Medical Resource Center for Next-Generation, Deployable Healthcare Designs

För omedelbar lansering

Anslut till oss


Browse Mouser's medical resource center
Browse Mouser's medical resource center

May 14, 2026Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, highlights its extensive medical resource center enabling deployable healthcare tools. This hub provides engineers and healthcare innovators with the resources to develop advanced medical technologies and stay informed on emerging trends shaping patient care.

Accelerated by the demand for connected and personalized healthcare, secure Wi-Fi® modules power Internet of Medical Things (IoMT) wearable devices, enabling continuous, real-time monitoring beyond traditional clinical settings. These innovations support more proactive, preventive care by allowing earlier intervention and reducing the need for hospital visits. Technologies like 3D printing and smart glasses further enhance personalization and clinical efficiency, delivering patient-specific implants and hands-free tools that improve accuracy, training, and remote collaboration.

At the same time, PFA power design ensures emerging therapies are both safe and reliable in real-world deployment. With efficient machine learning models and embedded sensors, engineers can also bring intelligence to everyday health products, such as toothbrushes, toilets, and other consumer devices, enabling local data processing that improves privacy, responsiveness, and user experience. Together, these advancements are driving a shift toward more decentralized, data-driven healthcare that improves outcomes, reduces strain on the system, and expands access to quality care.

Curated by Mouser's technical team and trusted manufacturing partners, the medical resource hub offers content including articles, blogs, eBooks, and new products for medical technology from top manufacturers. Also featured is the Digital Therapeutics Puts Healthcare in Your Hands infographic, which highlights how software and connected devices are becoming clinically validated care tools that expand access, lower costs, and support personalized treatment beyond traditional settings. Readers will also have access to Mouser's New Tech Tuesdays, which provides engineers with insights into how innovations in AI, hardware security, and biometric technologies are driving the development of smaller, faster, and more efficient medical devices.

For the newest products, Mouser stocks the industry's widest selection of semiconductors and electronic components, including the newest solutions for medical applications. Featured products include:

  • The ST1VAFE6AX by STMicroelectronics is a compact biosensor for wearables and digital health devices that combines biopotential sensing with motion tracking in a single chip. It features a vertical analog front-end (vAFE) for single-ended or differential biopotential inputs, embedded sensor-fusion, and a machine-learning core. Designed to capture signals such as heart rate, pulse, and ECG, while synchronizing those readings with motion data so developers can do more context-aware analysis.
  • The BL54L modules from Ezurio are a family of Bluetooth® LE Low Energy modules built on Nordic's nRF54L platform, designed for secure, high-performance, low-power wireless connectivity in compact embedded devices. This series is made for engineers who want a ready-made BLE module that balances performance, miniaturization, and security without having to build the RF design from scratch.
  • The AR0145CS Hyperlux™ SG image sensors from onsemi are built for applications that need fast, accurate capture of moving scenes without motion distortion. These 1MP image sensors use a 1280 × 800 active-pixel array and are optimized for clear, low-noise imaging in both low-light and bright conditions. The AR0145CS sensors are applicable in barcode scanners, gesture recognition, 3D scanning, positional tracking, iris scanning, augmented and virtual reality, biometrics, and machine vision.
  • The FXLS8971CF  3-axis MEMS accelerometer by NXP Semiconductors is designed for medical and IoT applications that need reliable motion and orientation sensing with stable performance across temperature. This accelerometer supports both high-performance and low-power modes, enabling flexible trade-offs between accuracy and battery life. At the same time, its integrated digital features simplify host data collection and reduce overall system power consumption.

To browse Mouser's medical resource center, visit https://resources.mouser.com/medical/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764