Mouser Electronics Equips Electronic Design Engineers with Leading Medical Tech Resources and Products

För omedelbar lansering

Anslut till oss


September 25, 2024Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, is exploring the lifesaving technologies revolutionizing medical and healthcare industries through its dynamic medical resource center. With the latest prolific digital transformations, healthcare systems have felt groundbreaking advancements, enabling faster, more accurate diagnoses, reducing wait times, and adopting cutting-edge digital therapies. The analytical capabilities of artificial intelligence (AI) are reshaping patient care, offering unprecedented insights into health data, and transforming the approach to chronic illnesses and incurable diseases.

The expansive library of resources gives design engineers the tools to develop accurate and precise technologies to improve patients' lives. With dozens of articles, blogs, eBooks, and products, readers will find innovations transforming traditional healthcare and medicine.

Advances in technology have revolutionized patient outcomes, from early disease detection to personalized treatments. Wearable robotics are empowering those with limited mobility, enabling longer walks and enhancing quality of life. Meanwhile, thermal imaging is redefining healthcare by detecting heat anomalies invisible to the human eye, providing crucial insights that help patients make informed decisions and seek proactive treatments. As technology continues to evolve, we can expect to see even more medical advancements that will shape the future of healthcare and enhance human well-being.

Mouser stocks the industry's widest selection of semiconductors and electronic components, including the following new products and solutions for medical applications:

  • The SFH 7018x MULTILED® from ams OSRAM features three-in-one, high-performance multi-emitters for green, red, and infrared target heart rate and SpO2 monitoring. It's suitable for digital diagnostic devices, vital sign monitoring, and wearables.
  • The ST1VAFE6AX biosensor from STMicroelectronics is designed for biopotential signal detection and motion tracking. It features smart FIFO up to 4.5KB and SPI/I2C and MIPI I3C®1 serial interface with main processor data synchronization. With embedded features and data processing for motion processing, this biosensor can be used in healthcare, wearables, portable devices, activity tracking, and well-being applications.
  • The CEM102 from onsemi is a small form factor sensor with low power consumption that facilitates further miniaturization and extended battery life across various applications. The CEM102 Analog Front End (AFE) is intended to be used together with the onsemi RSL15 Bluetooth®2 wireless microcontroller and can detect abnormal sensor conditions and host processor wake-up. It's best used in IoT sensor devices and wearables.
  • The CUS800M and CUS1000M AC-DC power supplies from TDK-Lambda feature medical certifications (2 x MOPP) required for B- and BF-type medical equipment. They offer a compact design in a 171 x 85 x 42.5 mm footprint, which can benefit medical, audio and visual, and communication technology applications.

To learn more, visit https://resources.mouser.com/medical/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764