Renesas DA14695MOD Multi-Core Bluetooth 5.2 Module, Now at Mouser, Delivers Best-in-Class Power Consumption for Feature-Rich Applications

För omedelbar lansering

Anslut till oss


November 16, 2023Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, the authorized global distributor with the newest electronic components and industrial automation products, is now stocking the DA14695MOD multi-core Bluetooth® 5.2 module from Renesas Electronics. Based on the SmartBond™ DA14695 Bluetooth Low Energy (LE) system-on-chip (SoC), the multi-core Bluetooth module brings together an Arm® Cortex®-M33 application processor with a floating-point unit, a cryptographic security engine, and advanced power management. The DA14659MOD module supports the development of advanced user interfaces and feature-rich applications, including beacons, proximity tags, low-power sensors, Internet of Things (IoT) devices, and industrial applications.

The Renesas DA14695MOD multi-core Bluetooth 5.2 module, now available at Mouser, features an optimized programmable sensor node controller, allowing sensor node operations and data acquisition without CPU intervention. Boasting seven power domains for power consumption efficiency, the DA14695's advanced power management unit enables it to run on primary and secondary batteries and power external devices through an integrated SIMO DC-DC controller. The module integrates all passives, an antenna, and a 32Mbit QSPI FLASH, as well as a wide range of both standard and advanced peripherals. The devices' integrated JEITA-compliant USB charger allows the modules to natively charge rechargeable batteries.

The DA14695MOD Module is supported by the DA14695MOD-00DEVKT-P SmartBond™ Dev Kit Pro. Featuring a hardware-loaded development board with an onboard debugger, the Dev Kit Pro supports software development, testing and debugging for applications including wearable devices, automotive solutions, and consumer electronics. The DA14695MOD-00DEVKT-P SmartBond Dev Kit Pro includes a development toolchain, source code examples, and detailed documentation.

To learn more about the DA14695MOD Multi-Core Bluetooth 5.2 Module, visit https://www.mouser.com/new/renesas/renesas-dialog-da14695-modules/.

To learn more about the DA14695MOD-00DEVKT-P SmartBond Dev Kit Pro, visit https://www.mouser.com/new/renesas/renesas-dialog-da14695-kit/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764