Mouser Announces Global Distribution Agreement with ProSoft Technology to Deliver Industrial Communication Solutions

För omedelbar lansering

Anslut till oss


Learn more about ProSoft Technology
Learn more about ProSoft Technology

January 12, 2026Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, today announces a new global distribution agreement with ProSoft Technology, a world leader in the design and manufacture of high-performance communication solutions for the Industrial Internet of Things (IIoT) sector. ProSoft's industrial communication products address connectivity, optimization, modernization, and migration challenges, enabling the update of legacy equipment and providing support for all major industrial protocols.

The ProSoft Technology PLX3x protocol conversion gateways, now available from Mouser, are powerful, cost-effective solutions for transferring data between devices that use different protocols. The PLX30 gateways offer multiple communication methods (Client, Server, Master, Slave, I/O connections, and messaging) to optimize communication. These industrial-rated gateways are stand-alone, DIN-rail mounted, and can provide up to four (4) isolated serial ports.

The PLX82 protocol conversion gateways feature dual Ethernet ports that allow different protocols to operate on separate subnets, seamlessly integrating systems, such as EtherNet/IP™, IEC 61850, Modbus TCP/IP, and PROFINET. The onboard SD slot (SD card optional) can be used for storing configuration files that facilitate recovery, transferring the configuration to another gateway, or for general configuration backup.

The AN-X3 and AN-X4 phase migration gateways are next-generation solutions designed to seamlessly bridge modern EtherNet/IP systems with legacy automation networks. These gateways offer a flexible and phased migration path for upgrading Reliance® AutoMax DCS/Remote I/O or transitioning from older PLCs, HMIs, and field devices.

The PLX51 modernization gateway provides connectivity to EtherNet/IP, Modbus® TCP/IP, or Modbus Serial networks for PROFIBUS DP networks by operating as a PROFIBUS DP slave. For easy integration with Rockwell Automation Controllers, the gateway and configuration software create dynamic analog input/output (AIO) tags based on user configuration, allowing the addition of logical tag names to the PLC project file and reducing programming time.

To learn more about ProSoft Technology, visit https://www.mouser.com/manufacturer/prosoft-technology/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om ProSoft Technology

2026 - ProSoft Technology was founded in 1990 with the goal of providing solutions that help global customers increase production, reduce downtime, and lower operating and maintenance costs. Their solutions specifically address challenges in Connectivity, Optimization, Modernization, and Migration across various industries.

ProSoft supplies industrial communication solutions that enable dissimilar automation control equipment to share information and transfer critical control data through both wired and wireless connectivity. Their products allow for a phased migration of legacy control systems to modern infrastructure and empower customers to remotely get the right data to the right person when needed. Additionally, ProSoft offers innovative solutions to help OEM customers optimize their machine performance. These solutions are built with industrial-grade cybersecurity and are central to the emerging Industrial Internet of Things (IIoT).

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764