New eBook from Mouser Electronics and onsemi Highlights the Benefits of Silicon Carbide Power Electronics

För omedelbar lansering

Anslut till oss


August 8, 2024Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, today announces a new eBook in collaboration with onsemi, exploring the use of silicon carbide (SiC) semiconductors for power system design.

SiC devices are revolutionizing power electronics with their superior material properties, enabling more efficient, compact, and sustainable power systems. In Enabling a Sustainable Future with Silicon Carbide Power Electronics, onsemi explores the benefits of SiC, its applications in electric vehicles and renewable energy, and the importance of choosing the right SiC partner. A trusted supplier of power solutions, onsemi offers high-quality SiC devices, a reliable supply chain, and comprehensive design support.

The eBook includes convenient links to select onsemi power products, such as the NTBG014N120M3P EliteSiC MOSFET. The NTBG014N120M3P is a 1200V M3P planer SiC MOSFET optimized for power applications. Planar technology works reliably with negative gate voltage drives and turns off spikes on the gate. This device is ideal for use in solar inverters, electric vehicle charging stations, energy storage systems, and switch-mode power supplies.

The NVBG1000N170M1 EliteSiC MOSFET, also available from Mouser, is a 1700V M1 planar device optimized for fast switching applications. This device is AEC−Q101 qualified and PPAP capable, making it ideal for use in electric vehicles (EV) and hybrid electric vehicles (HEV). In EVs and HEVs, the advantages of SiC devices translate into power solutions that are smaller, lighter, and more efficient. Less energy is wasted, leading to a reduction in the number of expensive batteries required.

The NCP51705 gate drive is designed to primarily drive SiC MOSFET transistors. To achieve the lowest possible conduction losses, the driver is capable of delivering the maximum allowable gate voltage to the SiC MOSFET device. By providing a high peak current during turn-on and turn-off, switching losses are minimized.

The NCP51560 isolated dual-channel gate driver is designed for fast switching to drive power SiC MOSFET power switches. Two independent galvanically isolated gate driver channels can be used in any possible configurations of two low-side, two high-side switches or a half-bridge driver with programmable dead time. The NCP51560 offers other important protection functions, such as independent under-voltage lockout for both gate drivers.

To read the new eBook from Mouser and onsemi, visit https://resources.mouser.com/manufacturer-ebooks/onsemi-enabling-a-sustainable-future-with-silicon-carbide-power-electronics-mg/.

To browse Mouser's entire manufacturer eBook library, visit https://resources.mouser.com/manufacturer-ebooks/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About onsemi

2026 - onsemi is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end markets, the company is accelerating change across megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world's most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764