Mouser Now Stocking onsemi NCN26010 Ethernet Controller, Providing Reduced Wiring and Costs

Nya produktlanseringar

Anslut till oss


June 5, 2023Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the NCN26010 Industrial Ethernet Controller from onsemi. This 10BASE-T1S Ethernet controller is designed to provide reliable multi-point communication in industrial settings.

The onsemi NCN26010 is a 10Mb/s, IEEE 802.3cg compliant device including a media access controller (MAC), a PLCA reconciliation sublayer (RS), and a 10BASE-T1S PHY, designed for industrial multi-drop Ethernet networks. The device can enable more than 40 nodes on a single twisted pair, exceeding five times the amount of nodes requested by the IEEE 802.3cg standard, reducing installation cost and set-up complexity. This PHY + MAC controller for 10BASE-T1S can connect to controllers, sensors and other devices without the need for an external MAC.

The NCN26010 reduces in-cabinet wiring up to 70% while significantly increasing bandwidth. In backplanes, it simplifies the layout and power distribution without impacting data rates or latencies. Many applications, such as elevators, will be able to increase data throughput over existing wiring with the device and, due to the ability to carry power over data cables, complex sensor networks can be built upon simple and low-cost cable runs.

The NCN26010 makes an ideal replacement for legacy point-to-point and multi-point industrial communication standards. The T1S MAC/PHY device can replace RS-485, CAN, RS-232, HART and others. As a result, greater data throughput is achieved over existing wiring, eliminating the need to re-pull wires which is often the greatest expense in a networking installation. The NCN26010 also features a proprietary enhanced noise immunity feature which is essential for installations in electrically noisy industrial environments.

The NCN26010 controller is supported by the NCN26010XMNEVB 10BASE-T1S MACPHY evaluation board, the NCN26010BMNEVB Adapter Board, and the NCN26010XMNEVK 10BASE-T1S SPE evaluation kit, all available from Mouser.

To learn more about the onsemi NCN26010 Industrial Ethernet Controller, visit https://www.mouser.com/new/onsemi/onsemi-ncn26010/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About onsemi

2026 - onsemi is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end-markets, the company is accelerating change in megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world’s most complex challenges and leads the way to creating a safer, cleaner and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764