New onsemi Image Sensors, Available from Mouser Electronics, Enable Machine Vision, VR/AR, Biometrics, and More
July 29, 2024 – Mouser Electronics, Inc., is a global authorized distributor of products from onsemi, a leading manufacturer of semiconductor-based solutions driving energy-efficient innovations. With over 17,000 onsemi products available to order, Mouser offers an ever-expanding selection of the manufacturer’s newest semiconductor solutions. onsemi offers a broad portfolio of industry-leading image sensors that satisfy the requirements of multiple applications, from wearables and consumer electronics to demanding industrial and automotive applications. In the first quarter of 2024, onsemi has released three new, innovative image sensors, all of which are available from Mouser.
The onsemi AR2020 is a 1/1.8-inch back-side illuminated (BSI) stacked CMOS digital image sensor with a 5120 × 3840 active-pixel array. This advanced sensor captures images in either linear or enhanced Dynamic Range (eDR) modes with a rolling shutter readout. The features of the AR2020 provide a powerful data-capturing device at the edge that can be programmed through several options to deliver optimal bandwidth at very low power. This image sensor is ideal for video conferencing, biometrics, and machine vision applications.
The AR0830 is a 1/2.9−inch BSI stacked CMOS digital image sensor with a 3840 × 2160 active-pixel array. Also featuring linear and eDR modes and rolling shutter readout, this device delivers excellent performance in low light and near-infrared (NIR) wavelengths. The AR0830 image sensor features multiple functional modes, including global reset release (GRR), trigger, context switching, and wake-on motion (WOM). This image sensor is targeted at industrial machine vision, virtual and augmented reality (VR/AR), smart access and retail analytics.
The AR0234CS CMOS digital image sensor offers a 1920 x 1200 active-pixel array in a 1/2.6-inch optical format. This sensor incorporates a new innovative global shutter pixel design optimized for accurate and fast capture of moving scenes at 120 frames per second, full resolution. The AR0234CS produces extraordinarily clear, sharp digital pictures with an industry-leading global shutter efficiency, and its ability to capture both continuous video and single frames makes it the perfect choice for a wide range of applications, including scanning, autonomous mobility, surveillance and industrial quality control.
To learn more about the AR2020 sensor, visit https://www.mouser.com/new/onsemi/onsemi-ar2020-image-sensors/. To learn more about the AR0830 sensor, visit https://www.mouser.com/new/onsemi/onsemi-ar0830-image-sensors/. To learn more about the AR0234CS sensor, visit https://www.mouser.com/new/onsemi/onsemi-ar0234cs-sensors/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
2026 - onsemi is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end markets, the company is accelerating change across megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world's most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.