Explore the Evolution of Robotics to Autonomy in New eBook from Mouser Electronics and onsemi

För omedelbar lansering

Anslut till oss


Read the new eBook from Mouser and onsemi
Read the new eBook from Mouser and onsemi

December 2, 2025Mouser Electronics, Inc., the New Product Introduction (NPI) leader empowering innovation, announces a new eBook in collaboration with onsemi, exploring the transformative impact of robotics in scale, capability, context, and more. What began as fixed industrial machines programmed for repetitive tasks are now evolving into mobile, intelligent systems capable of navigating the physical world with real-time awareness.

In Engineering the Future: The Sensors and Systems Powering Modern Mobile Robots, engineers from onsemi and experts from across the industry discuss the impact of autonomous mobile robots (AMRs), the transformative potential of physical AI, and how engineers can develop solutions that are efficient, high-performing, and scalable. The eBook also highlights relevant products from onsemi that can help facilitate this robotic evolution.

The AR0235 digital image sensor, part of onsemi's Hyperlux SG product family, is a 1/2.8−inch 2.3 MP CMOS digital image sensor with an active−pixel array of 1920 × 1200. It incorporates a new innovative global shutter pixel design optimized for accurate and fast capture of moving scenes at 120 frames per second, full resolution. Its ability to capture both continuous video and single frames makes it the perfect choice for a wide range of applications, including machine vision for AMRs, 3D scanning, AR/VR, and industrial quality control.

The NCV75215 ultrasonic sensor is an application-specific standard product (ASSP) designed to provide time-of-flight measurement for obstacle avoidance and parking assistance. Utilizing a piezoelectric ultrasonic transducer, the NCV75215 operates with high sensitivity and low noise, allowing the detection of obstacles from 0.25m to 4.5m. Additionally, the NCV75215 includes EEPROM memory for configuration settings and user data, ensuring reliable and customizable operation.

Both the automation and automotive industries have traditionally used the Controller Area Network (CAN) Protocol to connect their subsystems. However, as these systems evolve, they require higher data throughput, simpler wiring, and denser sensor integration. The NCN26000 Ethernet 10BASE-T1S transceiver, available to order, offers all physical layer features necessary to transmit and receive data over a single unshielded twisted pair. In addition, it provides noise immunity to values well above the IEEE T1S standard.

The NCS32100 Inductive Position Sensor is an absolute rotary encoder offering a full-featured controller and sensor interface for high-resolution, high-accuracy angular sensing up to 50 arcsec. The NCS32100 has flexible configuration capabilities, allowing connection to a variety of inductive PCB sensor patterns and offers a variety of digital output formats. Inductive sensing techniques have unique advantages over traditional position sensor solutions, including but not limited to temperature insensitivity, mechanical simplification, and insensitivity to contaminants like dust, water, oil, or metal particles.

To read the new eBook from Mouser and onsemi, visit https://resources.mouser.com/manufacturer-ebooks/onsemi-engineering-the-future-sensors-and-systems-powering-modern-mobile-robots-mg/.

To browse Mouser's entire manufacturer eBook library, visit https://resources.mouser.com/manufacturer-ebooks/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

About onsemi

2026 - onsemi is driving disruptive innovations to help build a better future. With a focus on automotive and industrial end markets, the company is accelerating change across megatrends such as vehicle electrification and safety, sustainable energy grids, industrial automation, and 5G and cloud infrastructure. onsemi offers a highly differentiated and innovative product portfolio, delivering intelligent power and sensing technologies that solve the world's most complex challenges and leads the way to creating a safer, cleaner, and smarter world. onsemi is recognized as a Fortune 500® company and included in the Nasdaq-100 Index® and S&P 500® index.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764