Mouser and NXP Share Insights on Security Risk and Regulatory Compliance at the Edge in New eBook

Nya produktlanseringar

Anslut till oss


May 08, 2025Mouser Electronics, Inc., the New Product Introduction (NPI) leader empowering innovation, today announces a new eBook in collaboration with a global semiconductor leader, NXP® Semiconductors, that explores the ongoing design challenges and solutions for creating secure, interconnected edge devices.

With the rapid increase of Internet of Things (IoT) devices, mobile devices, and diverse network points, security concerns have drastically increased. Emerging technologies rely on interconnected edge devices that share data in real time and are often deployed in remote or uncontrolled environments, opening up new vulnerabilities beyond traditional information technology infrastructures. In 7 Experts Discuss Managing Security Risk and Regulatory Compliance at the Edge, security specialists from NXP and other companies discuss security risk management, regulatory compliance, and strategies for meeting current and future requirements.

NXP has a long history in the field of cybersecurity and offers customers a broad portfolio of products and solutions, many of which are highlighted in the eBook. The NXP EdgeLock® secure authenticators, such as the EdgeLock A5000, available from Mouser, are ready-to-use, secure IoT authenticators. It provides a root of trust at the IC level, and it gives an IoT authentication system state-of-the-art security capability right out of the box. The device is versatile in IoT security use cases, such as secure connection to public and private clouds, device-to-device authentication, and counterfeit protection.

The MCX N series microcontrollers are compact, secure, high-performance MCUs with an integrated NPU to enable scalable and innovative designs for the next generation of smart and secure connected devices in industrial and IoT edge applications. The devices feature advanced security with an integrated EdgeLock Secure Enclave(Core Profile) and are supported by NXP's EdgeLock 2GO cloud services for secure provisioning.

The EdgeLock SE050 secure element (SE) product family provides a trust anchor in IoT devices. This ready-to-use secure element offers enhanced Common Criteria EAL 6+ AVA_VAN.5 certified security for strong protection against the latest attack scenarios and an extended feature set for a broad range of IoT use cases.

The i.MX 93 applications processors provide power-provide efficient machine learning (ML) acceleration and advanced security with integrated EdgeLock Secure Enclave (Advanced Profile) to support energy-efficient and secure edge computing.

To read the new eBook, visit https://resources.mouser.com/manufacturer-ebooks/nxp-7-experts-discuss-managing-security-risk-and-regulatory-compliance-at-the-edge-mg/. To learn more about NXP, visit https://www.mouser.com/manufacturer/nxp-semiconductors/.

To browse Mouser's extensive eBook library, visit https://resources.mouser.com/manufacturer-ebooks/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764