Nexperia NBM5100A/B and NBM 7100A/B Battery Boosters Greatly Extend Battery Life and Performance for IoT Apps, Now at Mouser

Nya produktlanseringar

Anslut till oss


August 16, 2023Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now stocking the NBM5100A/B and NBM7100A/B battery boosters from Nexperia. Complementing the company's expanding battery management solutions portfolio, the new NBM5100A/B and NBM7100A/B battery boosters are ground-breaking battery life boosting ICs that extend the life of non-rechargeable Lithium primary batteries by up to 10x over competing solutions while also increasing peak output current by up to 25x compared to batteries without a battery booster. When coupled with the NBM5100A/B and NBM7100A/B, Lithium primary batteries will not only have a longer life, but the batteries will achieve higher performance, avoid unwarranted waste and be a better, more sustainable power source for low-power IoT and other portable applications that, before, could only operate using AA- or AAA- batteries.

The Nexperia NBM5100A/B and NBM7100A/B battery boosters, available from Mouser Electronics, are equipped with two high-efficiency DC/DC conversion stages and an intelligent learning algorithm to help better control the relatively high internal resistance and chemical reaction rates typically found with 3 V CR2032 and CR2025 Lithium coin cell batteries. The first conversion stage involves the slow energy transfer from the battery to a capacitive storage element. The second stage uses the conserved energy to provide a regulated (programmable from 1.8 V to 3.6 V) high-pulse output current (up to 200 mA). The intelligent learning algorithm monitors the energy consumed during repetitive load pulse cycles and optimizes the first DC/DC conversion stage to minimize the capacitor's residual charge. When not undergoing a cycle of energy conversion (standby state), the NBM5100A/B and NBM7100A/B consume less than 50 nA.

Each device features a peripheral interface for host communications, configuration and control. The NMB7100A and NBM5100A include an I2C interface, while the NMB7100B and NBM5100B offer a Serial Peripheral Interface (SPI). In addition, the NBM5100A/B incorporates a capacitor voltage balancing port for supercapacitor-based applications. Other features of the NBM5100A/B and NBM7100A/B include a low battery indicator/integrated fuel gauge, an auxiliary regulated output pin and brownout protection to prevent the storage capacitor from charging when the battery is nearing its end of life.

Extending the lifetime of energy-dense Lithium primary batteries, such as coin cells, Lithium thionyl (i.e., LS14250 1/2 AA) and emerging paper-printed battery types, the Nexperia's NBM5100A/B and NBM7100A/B battery boosters are available in a compact, 16-pin DHVQFN package measuring 2.5 mm x 3.5 mm x 0.85 mm. These ICs are specified over a temperature range of -40°C to +85°C, making them ideally suited for commercial indoor and industrial outdoor environments. Target applications include battery-powered wireless IoT nodes (Bluetooth®, LoRaWAN®, Sigfox™, LTE-M, NB-IoT, Zigbee®, etc.), wireless sensors, industrial devices, portable consumer devices, wearables and utility meters.

To learn more, visit https://www.mouser.com/new/nexperia/nexperia-nbm5100a-b-nbm7100a-b-boosters/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Nexperia

2026 - Nexperia, headquartered in the Netherlands, is a global semiconductor company with a rich European history and over 12,500 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every electronic design in the world – from automotive and industrial to mobile and consumer applications.

The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764