Authorized Distributor Mouser Electronics Spotlights Latest from Nexperia in Discretes, Power and MOSFET Devices

För omedelbar lansering

Anslut till oss


September 19, 2023Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, is stocking the latest innovations from Nexperia, a leading global high-volume manufacturer and supplier of discretes, logic and MOSFET devices. A winner of Nexperia's "2022 E-Tailer of The Year" award, Mouser continues to expand its customers' product development process by offering more than 13,000 parts from Nexperia.

Nexperia's extensive portfolio, available from Mouser, includes diodes, bipolar transistors, electrostatic discharge (ESD) protection devices, MOSFETs, GaN FETs and analog and logic ICs that meet stringent automotive industry standards. These products are recognized as benchmarks in efficiency, process, size, power and performance, with industry-leading energy and space-saving packages.

Some of the newest Nexperia products available from Mouser include the Nexperia NEH2000BYJ energy harvesting power management integrated circuit (PMIC). This high-performance energy harvesting solution for low-power applications collects energy generated by ambient sources, such as light, to charge storage elements such as rechargeable batteries or hybrid supercapacitors– thereby eliminating the need for battery swaps. Nexperia's Maximum Power Point Tracking (MPPT) uses an embedded hill-climbing algorithm to deliver maximum power to the load, independent of specific characteristics of the harvesters. The NEH2000BY does not require any inductor to function, allowing for a reduced BOM cost and a simpler system design for product designers. The companion NEVB-NEH2000BY evaluation boards allow convenient evaluation of the NEH2000BY energy harvesting PMIC. The boards offer a small form factor for easy integration into prototype applications.

The Nexperia NBM5100A/B and NBM7100A/B battery life booster ICs are designed to remove the limitations associated with coin cell batteries to enhance performance. Nexperia Battery Management ICs extend the life of a typical non-rechargeable lithium coin cell battery by up to 10x compared to competing solutions while also increasing its peak output current capability by up to 25x. The NBM5100A and NBM7100A offer support for I2C interfaces, and the NBM5100B and NBM7100B provide support for SPI interfaces, allowing for design flexibility.

Nexperia eMode GaN FETs offer voltage ranges of 100V to 650V with superior switching performance. These FETs deliver fast transition and switching capability and excellent power efficiency with low QC and QOSS values. Nexperia Low Voltage (< 200V) eMode GaN FETs provide optimum flexibility in power systems, enabling faster charging for e-mobility and wired / wireless changing systems, as well as significant space and BOM savings in LiDAR and low noise in Class D audio amplifiers.

To learn more about all the Nexperia products available at Mouser, visit https://www.mouser.com/manufacturer/nexperia/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Nexperia

2026 - Nexperia, headquartered in the Netherlands, is a global semiconductor company with a rich European history and over 12,500 employees across Europe, Asia, and the United States. As a leading expert in the development and production of essential semiconductors, Nexperia’s components enable the basic functionality of virtually every electronic design in the world – from automotive and industrial to mobile and consumer applications.

The company serves a global customer base, shipping more than 100 billion products annually. These products are recognized as benchmarks in efficiency – in process, size, power, and performance. Nexperia's commitment to innovation, efficiency, and stringent industry requirements is evident in its extensive IP portfolio, its expanding product range, and its certification to IATF 16949, ISO 9001, ISO 14001 and ISO 45001 standards.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764