Mouser Electronics New Product Insider: Over 15,000 New Parts Added in Second Quarter of 2025

Nya produktlanseringar

Anslut till oss


Learn more about Mouser's newest products
Learn more about Mouser's newest products

July 8, 2025Mouser Electronics, Inc., As an authorized distributor, Mouser Electronics, Inc. is focused on the rapid introduction of new electronic components and technologies, giving customers an edge and helping speed time to market. Over 1,200 semiconductor and electronic component manufacturer brands count on Mouser to help them introduce their newest products into the global marketplace. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each manufacturer.

Last quarter, Mouser launched over 15,000 new part numbers ready for shipment, with almost 10,000 introduced in April alone.

Some of the products introduced by Mouser from April through June include:

ROHM Semiconductor ML63Q2537 and ML63Q2557 Microcontrollers
The ML63Q2537 and ML63Q2557 microcontrollers (MCUs) feature a 32-bit Arm® Cortex®-M0+ processor and ROHM Semiconductor's proprietary AxlCORE-ODL AI accelerator. These MCUs provide on-device AI solutions for a wide range of edge computing applications. These devices also integrate a wide portfolio of peripheral circuits, including CAN FD controller, PWM for three-phase motor control, dual-unit A/D converters, analog comparators, I²C, SPI, and UART. With a low power consumption of approximately 40mW during AI processing, the ML63Q2500 Group is ideal for anomaly detection and predictive maintenance in industrial IoT (IIoT) equipment and home appliances.

Seeed Studio reCamera 2002 and 2002w AI Cameras
The reCamera 2002 and 2002w from Seeed Studio are pocket-sized, modular AI cameras powered by a RISC-V system-on-chip (SoC) running Linux. Featuring 1 TOPS @INT8, a 5MP camera, built-in YOLOv11, and support for custom AI models and Node-RED, easing the deployment of AI vision into any system. The 2002w variant includes 2.4/5 GHz Wi-Fi® and Bluetooth® 4.2/5.0 for wireless connectivity.

STMicroelectronics LSM6DSV320X 6-Axis Inertial Measurement Unit
The LSM6DSV320X 6-axis inertial measurement unit (IMU) by STMicroelectronics is designed to monitor and safeguard users in their individual surroundings and contexts. This IMU combines unmatched precision, embedded edge AI, and up to 320 g acceleration to enable applications like real-time fall detection for wearables, accident data recording, and goods monitoring.

Schneider Electric Altivar™ Machine Drive ATV320 Solar VSDs
The Altivar™ Machine Drive ATV320 solar variable speed drives (VSDs) provide a sustainable solution that harnesses the power of the sun without producing any CO2 emissions. The ATV solar VSDs are robust, simple to commission, and easy to integrate for pumping applications for agricultural, commercial, or industrial applications. Schneider Electric's free, user-friendly SoMove software simplifies device configuration to optimize the time spent in the field.

To see more New Product Insider highlights, visit https://info.mouser.com/new_products/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764