Mouser Electronics New Product Insider: Over 9,000 New Parts Added in First Quarter of 2026
April 15, 2026 – As an authorized distributor, Mouser Electronics, Inc. is focused on the rapid introduction of new products and technologies, giving customers an edge and helping speed time to market. Over 1,200 semiconductor, electronic component, and industrial automation manufacturer brands count on Mouser to help them introduce their products into the global marketplace. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each manufacturer.
Last quarter, Mouser launched more than 9,000 part numbers ready for shipment. Some of the products introduced by Mouser from January through March 2026 include:
- STMicroelectronics STM32C5 Arm® Cortex®-M33 Microcontrollers
The STM32C5 microcontrollers (MCUs) from STMicroelectronics are specifically designed to boost the performance of billions of tiny smart devices across factories, homes, cities, and infrastructure while meeting stringent cost, size, and power constraints. Based on ST's proprietary 40 nm manufacturing process, the STM32C5 MCUs can run tasks noticeably faster than many entry-level chips currently in use. This gives products more room to include features such as improved sensing, smoother control, and enhanced user experiences while keeping dynamic power consumption low. The MCUs also integrate security features that help safeguard products against tampering and cyber risks. - EDATEC ED-CM0NANO Single-Board Computer
The ED-CM0NANO is a single-board computer (SBC) from EDATEC, based on the Raspberry Pi Compute Module Zero (CM0). The ED-CM0NANO features a quad-core Arm Cortex-A53 processor running at up to 1 GHz, a Broadcom VideoCore-IV graphics processor, and a wide range of connectivity options. Optional Wi-Fi® support with an external antenna enables wireless connectivity, while integrated real-time clock (RTC) and watchdog timer enhance system reliability. These features make the ED-CM0NANO ideal for industrial control systems and Internet of Things (IoT) applications. - Sensata Technologies MGD Resonix™ Refrigerant Leak Sensor
The MGD Resonix™ sensor from Sensata delivers high accuracy and fast response times in a compact module designed to fit into the most compact heating, ventilation, air conditioning (HVAC), and refrigeration equipment. The MGD series offers superior resistance to overexposure and poisoning, as well as to high temperatures (working temperatures up to 105 °C) and humidity. These devices also have a service life of more than 15 years with no need for calibration, making them the ideal leak-detection component for A2L HVAC and refrigeration systems. - u-blox ANN-MB3 Triple-Band GNSS Antenna
The ANN-MB3 antenna from u-blox is a best-in-class L1/L2/L5 triple-band RTK real-time kinematic (RTK) solution ideal for the F20 high-precision GNSS platform. Optimized for seamless integration, the ANN-MB3 antenna delivers exceptional performance with a robust design. The antenna's compact (62 × 80 × 25.5 mm) form factor and flexible installation options enable the adoption of high-precision positioning technologies across industrial, automotive, and robotics applications.
To see more of the New Product Insider highlights, go to https://info.mouser.com/new_products/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.
2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.
Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.