Mouser Now Shipping the Murata Type2BP Ultra-Wideband Module for Wireless IoT Applications

För omedelbar lansering

Anslut till oss


July 13, 2023Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now shipping the Type2BP ultra-wideband (UWB) module from Murata. The Type2BP UWB module is ideal for the wireless enablement of larger infrastructures including access control, indoor positioning anchors and payment terminals, as well as consumer products, such as televisions and gaming consoles.

The Murata Type2BP UWB module, available from Mouser Electronics, is ideal for the growing ecosystem of spatial context awareness in IoT devices while simplifying wireless development by minimizing the amount of RF expertise needed to wirelessly enable a wide range of applications. The Type2BP module is one of the smallest (6.6 mm × 5.8 mm × 1.2 mm) UWB module available on the market and is based on NXP Semiconductors’ SR150 UWB chipset, clock, filters and peripheral components. It features low current consumption and includes channels 5 and 9 support with enhanced and secure ranging along with various antenna support configurations (3D angle of arrival (AOA) or 2D AOA).

The Type2BP UWB module also features integrated physical layer (PHY) and medium access controller (MAC) functions designed to meet FiRa™ specifications, to ensure interoperability with a growing set of UWB devices.

The Murata Type2BP UWB module is supported by the UWB-Module-EVK evaluation kit, also available at Mouser. This kit consists of an integrated evaluation board featuring the Type2BP UWB module, the NXP QN9090 Bluetooth® Low Energy SoC (system on a chip) and a USB / JTAG interface. The kit is powered through a USB cable from a PC and includes an integrated onboard PCB pattern patch antenna, a power circuit, an SWD connector and a level shifter. This development kit is approved by Apple® for the purpose of evaluating UWB-enabled accessories that leverage Apple's Nearby Interaction Framework for spatial location.

To learn more about the Murata Type2BP UWB module visit: https://www.mouser.com/new/murata/murata-type2bp-uwb-module/.

To learn more about the UWB-Module-EVK evaluation kit, visit https://www.mouser.com/new/murata/murata-type2bp-uwb-module-eval-kit/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Murata

2026 - Murata is a worldwide leader in the design and manufacture of ceramic passive electronic components, wireless connectivity modules, and power conversion technologies. Since its establishment in Kyoto in 1944, Murata has contributed to the advancement of society and the evolution of the electronics industry. The company's innovations can be found in a wide range of applications: mobile phones, home appliances, automotive electronics, energy management systems, healthcare devices, and more. Today, Murata is a global enterprise with over 100 offices worldwide. Aspiring to the slogan, “Innovator in Electronics®,” approximately 48,000 Murata employees strive every day to develop promising new technologies, “world’s first” innovations, and products shaping the future of electronics, all toward enabling customers to realize their vision.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764