Murata's New Type 2AB Ultra-Wideband Module, Now at Mouser, Delivers Exceptional Performance for Size- and Power-Sensitive Applications

Nya produktlanseringar

Anslut till oss


Month 23, 2023Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking the Type 2AB UWB+BLE combo ultra-wideband module from Murata Electronics, featuring both ultra-wideband (UWB) (channels 5 and 9) and Bluetooth® Low Energy (BLE) 5.2 RF technology. Offering low current consumption and a small form factor, the combo module supports a range of small, battery-operated applications, including Internet of Things (IoT) devices, connected tracking devices, industrial sensors and controllers, and condition monitoring solutions.

The Murata Type 2AB UWB+BLE ultra-wideband module, now available at Mouser, delivers an exceptional battery life of more than ten years in an ultra-small, 10.5 mm × 83 mm × 1.44 mm package. The module features an embedded reference clock and an integrated three-axis sensor, while sophisticated collaborative coexistence hardware mechanisms and algorithms ensure that WLAN and Bluetooth collaboration is optimized for maximum performance. The high-performance module is based on the NXP 88W9098 combo chipset, supporting Wi-Fi® 6 (802.11a/b/g/n/ac/ax) 2×2 MIMO and Bluetooth 5.3 BR/EDR/LE 2MPHY up to a 1200 Mbps PHY data rate on Wi-Fi and a 3Mbps PHY data rate on Bluetooth. The module's WLAN section supports the PCIe 2.0 interface with optional support for SDIO 3.0, while the Bluetooth section supports the high-speed four-wire UART interface and PCM for audio data.

The Type 2AB UWB+BLE module's low-power performance and small form factor make it an ideal choice for size- and power-sensitive applications, including handheld wireless systems, gateways, and video streaming solutions.

The Type 2AB UWB+BLE module is supported by the LBUA5QJ2AB-828EVB evaluation kit. The evaluation kit offers a complete test and development platform on a 47 mm × 80 mm PCB, with a pre-mounted Type 2AB module, onboard UWB and BLE antennas and all required support circuitry. USB Type-C™ connectors enable easy connection to power and a PC.

To learn more about the Type 2AB UWB+BLE combo ultra-wideband module, visit https://www.mouser.com/new/murata/murata-type-2ab-module/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Murata

2026 - Murata is a worldwide leader in the design and manufacture of ceramic passive electronic components, wireless connectivity modules, and power conversion technologies. Since its establishment in Kyoto in 1944, Murata has contributed to the advancement of society and the evolution of the electronics industry. The company's innovations can be found in a wide range of applications: mobile phones, home appliances, automotive electronics, energy management systems, healthcare devices, and more. Today, Murata is a global enterprise with over 100 offices worldwide. Aspiring to the slogan, “Innovator in Electronics®,” approximately 48,000 Murata employees strive every day to develop promising new technologies, “world’s first” innovations, and products shaping the future of electronics, all toward enabling customers to realize their vision.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764