Mouser Electronics and Murata Present New eBook Focused on Micro-Electromechanical Systems (MEMS) Technology

För omedelbar lansering

Anslut till oss


May 9, 2024Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, today announces a new eBook in collaboration with Murata, exploring the use of micro-electromechanical systems (MEMS) technology device design. In 9 Industry Experts Discuss MEMS Technology, industry thought leaders offer unique perspectives on the benefits and applications of MEMS technology in consumer electronics, medical, Internet of Things (IoT) and industrial implementations.

Chapters on inertial measurement units (IMUs) and MEMS-based leveling devices discuss how these sensors provide the ability to determine relative position and orientation. Another chapter discusses the differences between consumer and industrial-grade MEMS sensors. The eBook concludes with emerging trends in the field of MEMS technology, such as the integration of intelligence into solutions, miniaturization, and applications such as virtual reality (VR) and augmented reality (AR).

The eBook includes convenient links to select Murata MEMS sensors, such as the SCA3300-D01 3-axis accelerometer and inclinometer, which is designed to provide high accuracy measurement in challenging applications, with ultralow noise density, excellent stability, superior vibration robustness, and extensive self-diagnostics. This sensor is suitable for motion analysis and control, professional leveling, and navigation systems.

The SCL3400-D01 digital 2-axis inclinometer, based on Murata's capacitive 3D-MEMS process, is ideal for leveling and tilt-sensing applications, such as monitoring structural health. The SCR410T-K03 gyroscope and SCC433T-K03 gyroscope and accelerometer, part of Murata's SCC400T series, are ideal for applications requiring high stability in harsh environments. Industrial applications include robotic control systems, machine control systems, platform stabilization and control, and motion analysis and control.

To learn more about Murata products available from Mouser, visit https://www.mouser.com/manufacturer/murata/.

To read 9 Industry Experts Discuss MEMS Technology, visit https://resources.mouser.com/manufacturer-ebooks/murata-9-industry-experts-discuss-mems-technology-mg/.

To browse all of Mouser's manufacturer eBooks, visit https://resources.mouser.com/manufacturer-ebooks/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Om Murata

2026 - Murata is a worldwide leader in the design and manufacture of ceramic passive electronic components, wireless connectivity modules, and power conversion technologies. Since its establishment in Kyoto in 1944, Murata has contributed to the advancement of society and the evolution of the electronics industry. The company's innovations can be found in a wide range of applications: mobile phones, home appliances, automotive electronics, energy management systems, healthcare devices, and more. Today, Murata is a global enterprise with over 100 offices worldwide. Aspiring to the slogan, “Innovator in Electronics®,” approximately 48,000 Murata employees strive every day to develop promising new technologies, “world’s first” innovations, and products shaping the future of electronics, all toward enabling customers to realize their vision.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764