Mouser Electronics, T-Works Partner to Boost India’s Hardware Innovation Ecosystem

Mouser Electronics to Fund State-of-the-Art Prototyping Facilities at T-Works
För omedelbar lansering

Anslut till oss


T-Works building

December 21, 2021 - Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, proudly announces a partnership with T-Works, an initiative by the Telangana State Government to sponsor state-of-the-art prototyping facilities. Through the partnership, Mouser Electronics will be an electronics and semiconductor components technology partner, supporting T-Works for the procurement of high-end prototyping equipment in the electronics test and measurement fields. This agreement follows multiple partnerships between the two entities over the years, culminating in what is Mouser’s largest contribution to date in India.

T-Works Phase 1, a 78,000 square-foot prototyping facility in Hyderabad, will be equipped with over 250 professional tools. The facility will enable innovators, startups, SMEs, and businesses to convert their ideas into industry grade physical products efficiently and economically. The Telangana State Government has, in total, allocated 4.79 acres for a 240,000 square feet T-Works prototyping center, which will be taken up in phases.

Sujai Karampuri, CEO of T-Works, said, “Phase 1 of T-Works is almost complete and equipment procurement is underway. We are excited about this partnership with Mouser and the potential benefits it brings towards accelerating innovation for hardware product development in India. Our partnership with Mouser began with subsidized components procurement and providing vital support for sourcing key parts during the pandemic. It has now transformed into Mouser’s largest contribution to date anywhere in India. This is a major validation from the industry of the impact T-Works will have in India’s product development ecosystem.”

“Through this partnership with T-Works, we aim to support innovators with the resources they need to solve tomorrow’s challenges,” added Mark Burr-Lonnon, Mouser Senior Vice President of Global Service & EMEA and APAC Business. “At Mouser, we’re eager to share our industry expertise through a steady stream of informative content along with the newest product lines to support engineers in all stages of the design process.”

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764