Mouser Electronics Breaks Ground on Major New Expansion of Global Distribution Center

För omedelbar lansering

Anslut till oss


Mouser combines exceptional warehouse logistics, leading-edge automation, and people power to get designers the parts they need to speed time-to-market.

August 16, 2022Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is greatly expanding its large global headquarters and distribution center to continue meeting the needs of its flourishing business well into the next decade. The company recently broke ground on a 416,000-square-foot, three-story building that will expand its distribution center, located south of Dallas-Fort Worth, Texas.

“With a larger warehouse space and continuing investment into automation and staffing, Mouser is preparing for the future while ensuring the highest levels of customer service today,” says Pete Shopp, Mouser Electronics’ Senior Vice President of Business Operations. “The tools and systems we’ve put in place offer another way we can help shorten our customers’ time to market.”

Upon completion of the new construction, Mouser’s 78-acre global headquarters and massive distribution center will consist of almost 1.5 million square feet to accommodate Mouser's vast inventory of 1 million unique SKUs for products and technologies from over 1,200 electronic component manufacturers. The new building will feature a triple-mezzanine floorplan, advanced automation, and a skybridge connector to the existing distribution center building. Altogether, the new addition will solidify Mouser’s place as having some of the most advanced receiving, order pulling, and shipping departments in e-commerce. For an extensive look into how Mouser combines exceptional warehouse logistics, leading-edge automation, and people power, go to https://www.mouser.com/video/?play=6304627371001.

In spring 2022, Mouser completed installation of 120 vertical lift modules (VLMs), the largest VLM installation in the world. VLMs are essentially giant vertical filing cabinets, complete with shelves and an automated extractor to bring the components to the employee’s workstation. This increases efficiency and floor space and can reduce an employee’s walking time by 45% or more.

In addition to the massive VLM installation, Mouser’s distribution center features multiple Ultipack and I-Pack machines — a sophisticated automated system for sealing and labeling shipments that can process up to 14 orders per minute — as well as an OPEX Perfect Pick system for consolidation and an AutoStore system.

Though the adoption of start-of-the-art automation acts primarily as a means of boosting efficiency, productivity, accuracy and speed, the systems also enable more sustainable operations and improved customer satisfaction.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764