Mouser Electronics’ State-of-the-Art Distribution Center Features World’s Largest Installation of Vertical Lift Modules

För omedelbar lansering

Anslut till oss


Vertical Lift Modules in the Mouser Distribution Center

February 21, 2022Mouser Electronics, Inc., the industry’s leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, continues its investment in state-of-the-art automation in its global distribution center to increase order processing, accuracy and speed, helping customers further reduce time-to-market.

This spring 2022, Mouser will have 120 vertical lift modules (VLMs) installed, the largest VLM installation in the world. VLMs are essentially giant vertical filing cabinets, complete with shelves and an automated extractor to bring the components to the employee’s workstation. This increases efficiency and floor space and can reduce an employee’s walking time by 45% or more.

In addition to the massive VLM installation, Mouser’s distribution center features multiple Ultipack and I-Pack machines — a sophisticated automated system for sealing and labeling shipments that can process up to 14 orders per minute — as well as an OPEX Perfect Pick system for consolidation and an AutoStore system.

“Incorporating the latest in distribution center automation helps us meet our goal of providing exceptional customer service,” says Pete Shopp, Mouser Electronics’ Senior Vice President of Business Operations. “The tools and systems we’ve put in place offer another way we can help shorten our customers’ time to market.”

Mouser’s massive global distribution center, located on the 78-acre campus of its corporate headquarters in the Dallas-Fort Worth Metroplex, handles a vast inventory of more than 1 million unique SKUs for products from over 1,200 manufacturer brands. Processing tens of thousands of orders weekly — most within 15 minutes — and maintaining a strong commitment to customer service, Mouser employees are handling the technological advancements with great success.

Though the adoption of start-of-the-art automation acts primarily as a means of boosting efficiency, productivity, accuracy and speed, the systems also enable more sustainable operations and improved customer satisfaction.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764