Mouser Electronics Shares Expert Design Solutions for Advanced Robotics Development in New Interactive eBook from Molex

Nya produktlanseringar

Anslut till oss


Read "The Electric Workforce" Interactive eBook
Read "The Electric Workforce" Interactive eBook

August 6, 2025Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, today announces a new interactive eBook in collaboration with electronics manufacturer and connectivity innovator Molex.

In The Electric Workforce, the new interactive eBook examines how advances in connectivity, power management, and user interfaces are propelling robotics from the factory floor to household and commercial use. Reliable connectors, sensors, and real-time processing enable these robots to navigate, interact, and perform tasks efficiently in everyday environments. The eBook includes articles, videos, and an interactive infographic detailing the ways in which robotics will become ubiquitous in our everyday lives.

The eBook details the challenges designers face in building personal and home robots. These robots will need to interact with humans using voice commands, touchscreen controls, and apps. They will also need to be capable of autonomous mapping and developing efficient, safe routes to complete their tasks while optimizing battery life. The underlying technologies, such as chargers, sensors, processors, and actuators, require effective, reliable interconnect components and assemblies to carry power and signal throughout each robot. Molex offers a comprehensive line of interconnect products, available from Mouser, to facilitate manufacturing and ensure reliability throughout the robots' life cycle.

The Molex Premo-Flex flat flexible cable (FFC) Jumpers enable designers to maximize PCB space, reduce component costs, and provide devices with reliable board-to-board connections, making them well-suited for robotic applications. The series is offered in lengths, pitches and circuit sizes designed to solve complex board-to-board interconnection challenges in compact or hard-to-reach applications.

The MX150 mid-voltage connectors are designed to meet the growing demand for 48V electrical systems. Part of the extended Molex MX150 connector family, this sealed connector system is field-proven and offers highly reliable performance under extreme temperatures, varying degrees of vibration, and exposure to moisture and chemicals for a variety of applications.

The Squba 1.8mm/3.6mm sealed wire-to-wire connectors feature a protected, low-profile positive latch to reduce the overall component size, while the 1.8 mm pitch further alleviates space constraints. Molex Squba connectors have a contact resistance of 10 milliohms and are ideal for a wide range of space-constrained applications such as robotics and industrial controls.

To read the new eBook, visit https://www.mouser.com/molex-electrification-ebook/. To learn more about Molex products available from Mouser, visit https://www.mouser.com/manufacturer/molex/.

To browse Mouser's extensive eBook library, visit https://resources.mouser.com/manufacturer-ebooks/.

For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

 

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764