New eBook from Molex and Mouser Highlights New Innovations in Medical Device Design

För omedelbar lansering

Anslut till oss


March 7, 2022Mouser Electronics, Inc., the New Product Introduction (NPI) leader™ empowering innovation, announces a new eBook in collaboration with Molex, exploring the newest solutions and applications at the intersection of connectivity and medical device design. In Improving Lives with Digital Healthcare, leading experts from Molex and Mouser offer in-depth articles examining the next generation of digital healthcare solutions, including robotic surgery, medical wearables, brain-computer interfaces, and medical training with immersive technologies.

Today’s medical devices bring together a diverse range of sensors, connectivity solutions, and cable assemblies to deliver key advances in diagnostic, monitoring, and therapeutic treatments. Improving Lives with Digital Healthcare, the new eBook from Mouser and Molex, helps to untangle the complexities of digital healthcare, offering usable resources for designing new devices. The eBook features an article on emerging connectivity solutions for robotic surgery, including the use of optical fiber technology to support laser therapy. The eBook also examines the growing field of brain-computer interface applications, in which artificial intelligence and sensor hubs could one day lead to “superhuman” cognition.

Improving Lives with Digital Healthcare features product information for 15 Molex devices, connecting readers directly to the tools needed for next-generation medical applications. The Molex ISM standalone antennas provide an antenna volume reduction of up to 75% compared with conventional designs, as well as dual-band operation at 868 MHz and 915 MHz. The compact antennas can be easily integrated into telehealth devices, microwave ablation machines, diathermy therapeutic devices, and more. The 0.25 mm-pitch Premo-Flex jumpers deliver durable, ultra-flexible solutions for PCB connections in patient monitoring, telehealth, and surgical equipment. The compact jumpers feature a maximum current of 0.2 A and are ideal for tight packaging applications.

Mouser offers an ever-broadening selection of the newest Molex products, with over 30,000 Molex parts in stock. To learn more about Molex, visit https://www.mouser.com/manufacturer/molex/. To read the new e-book, go to https://www.mouser.com/news/molex-improving-lives-with-digital-healthcare/molex-improving-lives-with-digital-healthcare.html.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764