Authorized Distributor Mouser Electronics Stocks Extensive Selection of Molex Products

För omedelbar lansering

Anslut till oss


May 15, 2025Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is the authorized global distributor with an extensive selection of solutions from Molex, a global electronics leader and connectivity innovator. As a leading global provider of connector solutions, Molex brings engineering excellence, trusted relationships, and an unparalleled commitment to quality and reliability. With more than 180,000 Molex products available to order, including over 35,000 in stock and ready to ship, Mouser offers a wide portfolio of Molex solutions for use in communications, data centers, transportation, medical, and industrial applications.

The Molex NextStream connector system, available from Mouser, offers next-generation data rates of up to 64Gbps PAM-4, meeting the PCIe Generation 6 standard. The NextStream system is designed to enable data centers to upgrade and meet the demands of data-intensive applications like artificial intelligence (AI), NVMe-EDSFF storage, CXL, UPI systems and high-performance computing. The NextStream system offers vertical, right-angle and side-exit cable designs that provide flexibility in PCB design, with multiple options including 4x, 8x, 16x, vertical and right-angle connectors.

The Molex Multi-Trak I/O connectors have been engineered to offer a solution that conserves space while providing high-speed data transmission capabilities. These connectors incorporate a combined design that includes signal and power capabilities, enhancing adaptability within limited spaces and adhering to the small form-factor (SFF) TA-1033 standard. This innovative approach affords significant flexibility, which is paramount in managing complex data infrastructures.

Molex's HyperQube interconnect system delivers high power density and robust electrical performance, even under high current loads. The interconnect system features a mechanical keying scheme to ensure board mount receptacles are correctly placed and oriented on a printed circuit board (PCB) or busbar. 

The Molex Micro-Fit+ PCIe 5.0 connectors provide hybrid power and signal integration in a compact design, making them ideal for high-current, space-constrained applications. Their durable design, which features fully isolated cavities to protect the terminals from damage, is bolstered by high-performance materials such as high-current copper alloy, liquid crystal polymer, tin plating, and phosphorous bronze.

Mouser has also collaborated with Molex to create eBooks as a resource for design engineers. The most recent, Wired for Success, discusses the advantages of custom RF cables over off-the-shelf or DIY cables. Mouser and Molex have joined together to create online tools where designers can create custom cables to suit specific application needs. Mouser has a strong business relationship with Molex and has won multiple awards from the manufacturer. Together, they sponsor the DS PENSKE Formula E racing team and the Vasser Sullivan Lexus IMSA racing team.

To learn more about Molex products available from Mouser Electronics, visit https://www.mouser.com/manufacturer/molex/.

 

Som en globalt auktoriserad distributör erbjuder Mouser världens största sortiment av de senaste halvledarna och elektroniska komponenterna – i lager och redo för leverans. Mousers kunder kan förvänta sig 100 % certifierade originalprodukter som är helt spårbara från alla tillverkningspartner. För att underlätta kundernas design har Mousers webbplats ett stort bibliotek av tekniska resurser, inklusive ett Tekniskt resurscenter, tillsammans med produktdatablad, leverantörsspecifika referensutföranden, applikationsanmärkningar, teknisk konstruktionsinformation, konstruktionsverktyg, samt annan nyttig information.

Om Mouser

2026 - Mouser Electronics är en auktoriserad distributör av halvledare och elektroniska komponenter med fokus på snabba produktlanseringar från sina tillverkningspartners. Den globala distributörens webbplats, Mouser.com, betjänar globala elektronikkonstruktörer och köpare, är tillgänglig på flera språk och med flera valutor och saluför över 6,8 miljoner produkter från över 1 200 tillverkare. Mouser har 28 supportplatser över hela världen för att erbjuda kundservice av högsta klass på lokala språk och i lokala valutor och tidszoner. Distributören levererar till över 650 000 kunder i 223 länder/territorier från sin nästan 93 000 m² stora, ultramoderna anläggning i Dallas storstadsområde i Texas. Besök https://www.mouser.com, för mer information.

Varumärken

Mouser och Mouser Electronics är registrerade varumärken som tillhör Mouser Electronics, Inc. Alla övriga produkter, logotyper och företagsnamn som omnämns häri är varumärken som tillhör sina respektive ägare.

För ytterligare information, kontakta:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
För pressförfrågningar, kontakta:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764